17.1 Clock Distribution

Figure 17-1. Clock Distribution Block Diagram

The PIC32CK SG/GC clock system features are as follows:

  • Clock sources, that is oscillators controlled by OSCCTRL and OSC32KCTRL:
    • A clock source provides a time base that is used by other components, such as Generic Clock Generators. Example clock sources are the internal 48 MHz DFLL48M, Ultra Low-power 32 kHz RC oscillator, OSCULP32K, PLL and external oscillators XOSC and XOSC32K.
  • Generic Clock Controller (GCLK), which generates, controls and distributes asynchronous clocks consisting of:
    • Generic Clock Generators: These have programmable prescalers that can use any of the system clock sources. The Generic Clock Generator 0 generates the clock signal GCLK_MAIN, which is used by the CPU and Data Ram Tightly Coupled Memory, which in turn generates synchronous clocks.
    • Generic Clocks: These are clock signals generated by Generic Clock Generators. They are the Peripheral Channels and serve as clocks for the peripherals of the system. Multiple instances of a peripheral will typically have a separate Generic Clock.
  • Main Clock Controller (MCLK)
    • The MCLK generates and controls the synchronous clocks for the system. This includes the CPU, bus clocks (AHB (Advanced High-performance Bus), APB (Advanced Peripheral Bus) and AXI (Advanced eXtensible Interface)), as well as the Special Function Register interfaces of the peripherals. It contains clock masks that can turn on/off the user interface of a peripheral as well as prescalers for the CPU and bus clocks.

The following figure illustrates an example, where SERCOM0 is clocked by the DFLL48M (RC 48 MHz) in Open Loop mode. The DFLL48M is enabled, the Generic Clock Generator n uses the DFLL48M as its clock source and feeds into Peripheral Channel 19. The Generic Clock, also called GCLK_SERCOM0_CORE, is connected to SERCOM0 that supplies the functional logic clocks. The SERCOM0 interface, clocked by CLK_SERCOM0_APB, has been unmasked in the MCLK APB SERCOM0 mask register, MCLK.CLKMSK2.MSK7.

Figure 17-2. Example of SERCOM_0 Clock
To customize the clock distribution, refer to these registers and bit fields:
  • The source oscillator for a generic clock generator 'n' is selected by writing to the Source bit field in the Generator Control n, (n=0-15), register (GCLK.GENCTRLn.SRC).
  • A Peripheral Channel m can be configured to use a specific Generic Clock Generator by writing to the Generic Clock Generator bit field in the respective Peripheral Channel m register (GCLK.PCHCTRLm.GEN).
  • The Peripheral Channel number, m, is fixed for a given peripheral. See the Mapping table in the description of GCLK.PCHCTRLm, (i.e., GCLK Chapter).
  • The AHB/APB/AIX Peripheral BUS clocks are enabled and disabled by writing to the respective bit in the AHB/APB/AIX Mask register. The AHB/APB/AIX clocks are enabled and disabled by writing to the respective bit in the AHB/APB/AIX Mask register (MCLK.CLKMSK[0,1,2,3].MSKn). They are enabled by default on reset.