These bits select the input source for generating
the CRC, as shown in the table below. The selected source is locked until either the
CRC generation is completed or the CRC module is disabled. This means the CRCSRC
cannot be modified when the CRC operation is ongoing. The lock is signaled by the
CRCBUSY status bit. CRC generation complete is generated and signaled from the
selected source when used with the DMA channel.
| Value | Name | Description |
|---|
| 0x00 |
NOACT |
No action |
| 0x01 |
IO |
I/O interface |
| 0x02-0x1F |
- |
Reserved |
| 0x20 |
CHN |
DMA channel 0 |
| 0x21 |
CHN |
DMA channel 1 |
| 0x22 |
CHN |
DMA channel 2 |
| 0x23 |
CHN |
DMA channel 3 |
| 0x24 |
CHN |
DMA channel 4 |
| 0x25 |
CHN |
DMA channel 5 |
| 0x26 |
CHN |
DMA channel 6 |
| 0x27 |
CHN |
DMA channel 7 |
| 0x28 |
CHN |
DMA channel 8 |
| 0x29 |
CHN |
DMA channel 9 |
| 0x2A |
CHN |
DMA channel 10 |
| 0x2B |
CHN |
DMA channel 11 |
| 0x2C |
CHN |
DMA channel 12 |
| 0x2D |
CHN |
DMA channel 13 |
| 0x2E |
CHN |
DMA channel 14 |
| 0x2F |
CHN |
DMA channel 15 |