5.22 Monitor MVRP Statistics
The MVRP Statistics page shows receiver and per-port sFlow statistics.

The MVRP Statistics page has the following parameters:
- Port: The logical port for the settings contained in the same row
- Failed Registrations: The number of failed VLAN registrations on this switch port. Each port implementing the MVRP protocol maintains a count of the number of times it has received a VLAN registration request but has failed to register the VLAN due to lack of space in the Filtering Database.
- Last PDU Origin: The MAC address of the most recent MVRP PDU received on this switch port. MAC is 00-00-00-00-00-00 if the protocol is not enabled on that switch port, or if the port has not received any MVRP PDUs yet.