5.23 Monitor sFlow
The sFlow Statistics page shows receiver and per-port sFlow statistics.

The sFlow Statistics page has the following parameters:
- Receiver Statistics
- Owner: This field shows the current owner of the sFlow configuration. It considers one of the following three values:
- If sFlow is currently unconfigured/unclaimed, then Owner contains <none>
- If sFlow is currently configured through web or CLI, Owner contains <Configured through local management>
- If sFlow is currently configured through SNMP, Owner contains a string identifying the sFlow receiver
- IP Address/Hostname: The IP address or hostname of the sFlow receiver
- Timeout: The number of seconds remaining before sampling stops and the current sFlow owner is released
- Tx Successes: The number of UDP datagrams successfully sent to the sFlow receiver
- Tx Errors: The number of UDP datagrams that has failed transmission. The most common source of errors is invalid sFlow receiver IP/hostname configuration. To diagnose, paste the receiver's IP address/hostname into the Ping Web page (Diagnostics → Ping/Ping6)
- Flow Samples: The total number of flow samples sent to the sFlow receiver
- Counter Samples: The total number of counter samples sent to the sFlow receiver
- Owner: This field shows the current owner of the sFlow configuration. It considers one of the following three values:
- Port Statistics
- Port: The port number for which the following statistics applies
- Flow Samples: The number of flow samples sent to the sFlow receiver originating from this port
- Counter Samples: The total number of counter samples sent to the sFlow receiver originating from this port.