5.3.5.5 Accepted List by Bonded Device (ALB)

Format: ALB

Use command ALB to add all currently bonded devices to the accept list. Command ALB does not expect any parameter.

The random address in the accept list can be resolved with command ALB for connection purpose. If the peer device changes its resolvable random address, the RNBD451 module is still able to detect that the different random addresses are from the same physical device and, therefore, allows a connection from such a peer device. This feature is particularly useful if the peer device is an iOS or Android device that uses a resolvable random address.

DefaultNone
Example:ALB // Add all bonded devices to accept list
Response:AOK // Success