5.5.5 Set Event Indication Mask (SEIM, <hex16>)
Format:
SEIM, <hex16>
The RNBD451 module activates one GPIO_PIN_RA3 pin
to indicate that there are some changes in the monitoring indicators. When the MCU
detects the changes in the GPIO, the MCU sends a command to read what indicators the
change included. Therefore, the MCU can send further commands to read the corresponding
indicator status. The SEIM command masks events that target
monitoring.
Use the 2-bytes bit mask parameter to set monitoring indicators (see the following table).
|
Bit index |
Function |
|---|---|
1 | Link quality (RSSI) |
Others | Reserved |
| Example: | SEIM,0002 | // Set Event mask enable link quality |
| Response: | AOK
| // Success |
Err | // Syntax error or invalid parameter | |
|
Note: The PDS stores
these parameters. The parameters are effective immediately without a
reboot.
| ||