3 LAB 2: EVENTS - GPIO Events on Button press
and 2 Hz RTC output
The main objective of this hands-on Lab is to build a simple example
using the Event System, RTC periodic interrupt timer and some GPIO. The example involves
configuration in the DASHBOARD, PINMUX, CLOCKS config and EVENTS configurator screens.
Our basic use case is to generate event triggers using the SW0 button press
event and Periodic Interrupt from internal RTC running on 2 Hz frequency. Given the core
independent nature of these peripherals with the event system, once it is configured, no
further code needs to be run.
The following sub-sections in lab 2 will explain how to:
Create new project for ATtiny817
Xlained Pro
Configure EVENTS
Configure CLOCKS: 1 kHz
CLK_RTC, for simple calculation of 2 Hz out
Configure Dashboard:
Enable EVOUT signals and RTC Periodic Interrupt timer
Configure PINMUX: SW0, SW1
and LED pins
Export, run and visualize the
output in Atmel Studio IDE
Setup and Configure the Project
Given that we know the use case clearly, the Event System and RTC can be
added as requirements.
Info: START’s CREATE NEW
PROJECT allows you to filter by both SW and HW requirements,
then select a microcontroller (MCU) device (and board). On the left-hand
side you will enter MCU Requirements, while on the right-hand side
you will see the MCU’s, Devices and Boards, which match these
requirements. Note the MCU requirements are both HARDWARE and SOFTWARE,
i.e., that a given MIDDLEWARE works on that MCU.
Todo:
In the
SOFTWARE SEARCH, search
“EVENT”
Increment the number
required to 1. (You will see it in the RESULTS list.) Do the
same for RTC.
Check the
Show only boards check box in the MCU
filter side.
Select ATtiny817
Xplained Pro
Finally, click on
CREATE NEW PROJECT.
Result: Project opens in DASHBOARD view. EVENT SYSTEM and RTC drivers have
been added.
Tip: Access the
following video fore more details on how to configure the DASHBOARD.
Todo: Uncheck Show
system drivers to simplify the view.
Todo: Select the project named
“MY PROJECT” then click rename.
Tip: When START projects are exported, the default project name is
the name of the project component.
Event System Configuration
The Event System (EVSYS) enables direct peripheral-to-peripheral
signaling. It allows a change in one peripheral (the Event Generator) to trigger
actions in other peripherals (the Event Users) through Event Channels without
using CPU. The CPU continues to execute instructions while the channel system
operates in parallel.
The START as a code configurator tool supports two ways to configure the
Event System, i.e., via General UI for EVENT_SYSTEM_0 available on project dashboard
or via Event System Configurator screen.
In the described use case, our PERIPHERAL EVENT GENERATOR triggers
are SW0 on PB5, and the RTC Periodic Interrupt timer.
Let’s go straight to the EVENTS tab:
Todo: Click on the EVENTS tab
( symbol, on a low-resolution screen).
Info: User Button (SW0) is connected to
PB5.
Tip: Since a button
press is asynchronous to the MCU and the SW0 is connected to PB5, the
GENERATOR trigger will be Asynchronous Event
from PB5.
Todo: Find an appropriate EVENT CHANNEL for
Asynchronous Event from PB5. Using a mouse
click + hold or click +
drag, then make this connection.
Once the GENERATOR(Async Event from Pin PB5) is connected to the corresponding
CHANNEL (Async Event Channel 1), it’s time to go further
to connect the CHANNEL to the corresponding USERS.
Todo: Connect Async EVENT Channel
1. In turn Async Event Channel 1 to USER, PORTMUX Event
Output 0.
Figure 3-11. Events configuration of SW0 on PB5
Info:
The Periodic Interrupt Timer (PIT) can generate an interrupt
on every nth clock period (n can be selected from the value 4 to 32768)
and moreover the PIT uses the same clock source (CLK_RTC) as the RTC
function.
RTC PIT: Our objective is a 2 Hz signal. We will set
the RTC_CLK to 1024; an appropriate GENERATOR trigger is Periodic
Interrupt CLK_RTC div 512.
Connect GENERATOR (Periodic Interrupt CLK_RTC div 512) to a suitable
event CHANNEL (Async Event Channel 3). (Long click
or start dragging to see possible channels). In turn
connect the CHANNEL output (Async Event Channel 3) to the USER
(PORTMUX Event Output 1).
Result: The EVENT SYSTEM CONFIGURATOR is now
set up is as follows:
A button press generates an Asynchronous Event from Pin
PB5, triggering PORTMUX Event Output 0
(via Async Event Channel 1).
An RTC Periodic interrupt CLT_RTC div 512, triggers
PORTMUX Event Output 1 via (Async Event
Channel 3).
Warning: We will need to separately enable components and signals
used in the DASHBOARD. (RTC_CLK can be configured either in the DASHBOARD or
in CLOCKS config).
CLOCKS, DASHBOARD and PINMUX Configurators
Minor configuration updates are needed in a few of the other configuration
windows.
CLOCKS, DASHBOARD and PINMUX Configurators
Atmel START provides you with an independent configurator to configure, control,
distribute and pre-scale the clock signals from the available oscillators by
supporting both internal and external clock sources.
Todo: Click on the RTC clock configuration gear.
Select 32 KHz divided by 32 as the RTC Clock Source Selection.
Result: The RTC clock is now set to 1 Khz.
Selecting the RTC shows its clock connections.
DASHBOARD Configuration
For our two components, the RTC and Event System, we now need to enable what we have
used.
Todo: Click on RTC_0
component, then PITEN: Enable
Todo: Enable the EVENT_SYSTEM_0 Component Signals
EVOUT/0 and EVOUT/1:
Tip: The EVENT_SYSTEM_0 DASHBOARD exposes a low-level view of the
Event System configuration, which can help to understand the generated code,
to initialize the event system. View the Event System generated code by
clicking VIEW CODE, then navigating to ./src/evsys.c
Figure 3-12. DASHBOARD view of EVENT SYSTEM matches code generated, SW0 Event
configuration highlighted
PINMUX Configuration
The EVOUT pins need no further configuration. All that is required is to
configure the SW0 pin.
Todo: Configure PB5 as a Digital Input, enable
Pull-ups.
Export, Run and Visualize
Here we reach to the final sub-section where we will be exporting the
project (.atzip format) from START and import it into Atmel Studio
IDE. After importing the project we will compile, run and visualize the output in
serial port terminal via the Virtual COM port.
Todo: Go to EXPORT
PROJECT, name the project “EVENTS_SW0_PIT”, then click
DOWNLOAD PACK and import the project into Atmel
Studio 7.
Tip: Ways to open the
Import Atmel Start Project Wizard in Atmel Studio 7:
Drag and drop
.atzip onto Atmel Studio 7
File > Import > Atmel START project
Double-click on the
.atzip file, this will open a new instance of
Atmel Studio 7
Todo: Using the Import Atmel Start
Project Wizard, create a new project in Atmel Studio 7.
Tip: The default name
matches the name of the .atzip (named in the Export Project
window)
Result: Project is created. Note that
main.c is empty, besides a call to a function which
initializes the configured peripherals. The configuration of the Event
System can be seen in evsys.c.
Todo: Associate the project with
the connected debugger.
Todo: Click Start
Without Debugging () to program the MCU.
Info: The image below shows all the
relevant connections on the ATtiny817 Xplained Pro.
Todo:
Verify 2 Hz PIT EVENT using the LED0
Connect:PB2 EVOUT/1 RTC_PIT to PB4
LED0
Result: LED should flash at 2
Hz.
Todo:
Verify 2 Hz PIT EVENT using the Data Visualizer
Connect: PB6 DGI GPIO1 to PB2 EVOUT/1
RTC_PIC
Todo:
First connect to
DGI (Data Gateway Interface)
Enable the
DGI GPIO check box (if not already
enabled)
Double-click to add a
Graph
Drag the GPI
GPIO1 onto a new plot (Careful: Picture
shows GPIO0)
Click
Start
Tip: Later when we
add a second graph, you may need to click the sync button.
Todo:
Press
SPACE bar to pause the graph
Click Show
cursors
Align cursors to
measure frequency
Todo:
Verify Event on SW0 press
Connect: PB6 (DGI GPIO1) to PA2 SW0 (EVOUT/0)
Todo:
Data Visualizer:
Minimize
configuration of graph
Double-click to
add a second graph
Drag the GPI
GPIO0 onto a new plot
SPACE bar to
start graph again
Start pressing SW0
Result: The EVOUT/0 corresponds to stimulus on PB5
(SW0).
LAB 2 Summary
This is the end of LAB 2. To summarize, we setup and added the Event
system according to the required use case. There were minor configurations needed
for the CLOCK, DASHBOARD and PINMUX. For example, in the DASHBOARD we enabled the
EVENT OUT signals, as well as the RTC PIT, while the PINMUX pin PB5 was configured
as a digital input with pull-up enabled.
The project was exported, run and verified using the Data visualizer.
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.