4.1 Programming Executive Communication

The programmer and Programming Executive have a Host-Client relationship, where the programmer is the host programming device and the Programming Executive is the client.

All communication is initiated by the programmer in the form of a command. Only one command at a time can be sent to the Programming Executive. In turn, the PE only sends one response to the programmer after receiving and processing a command. The PE command set is described in Programming Executive Commands. The response set is described in Programming Executive Responses.