5.2 Enabling/Disabling a Node in a Device Tree

By default, all nodes in the Device Tree Source file for the SAM9X60 SoC are set to a Disabled state.

Figure 5-5. CAN Structure in the SAM9X60 .dtsi File

The following components can be enabled in the board-specific SAM9X60-Curiosity .dts file, which overrides the existing status in the .dtsi file during the merge process.

Figure 5-6. CAN Structure in the SAM9X60 .dts File