6 Appendix B: PKOB4 Recovery Method
When the MPLAB PICkit On-Board 4 is not responding (in rare cases), the user can recover
its operation by following these steps:
Warning: Only use this utility to restore the
hardware tool boot firmware to its factory state. Use only if the hardware tool no
longer functions on any machine.
- With the WBZ351 Curiosity Board still being powered, short the two pads for
approximately 10 seconds.
Figure 6-1. Location of Pads to Short - Open the latest version of MPLAB X. For more details, refer to Software Prerequisites.
- Go to Debug>Hardware Tool
Emergency Boot Firmware Recovery.
Figure 6-2. Hardware Tool Emergency Boot Firmware Recovery - Follow the directions on the
screen. This resets the tool back to the factory conditions.Note: For more details, refer to How to Use the Hardware Tool Emergency Boot Firmware Recovery Utility.