9 Sending OPC Commands to Stepper Motor (ICICLE Kit)
(Ask a Question)After establishing the connection between client and server through the OPC UA channel, perform the following steps to start or stop the stepper motor that is connected to the ICICLE Kit Mikrobus connector.
- From the Address Space pane, drag-and-drop the Stepper Motor Controls object into the Data Access View pane as shown in the following figure.
Figure 9-1. UAExpert Window - Stepper Motor Controls
Important: A Recursive Add Notes dialog appears. Click Yes and continue with the next steps. - All the functionality exported by Motor Control Board such as motor start, motor stop, and so on are made visible in the Data Access View pane as shown in the following figure.
Figure 9-2. UAExpert - Data Access View
The following table lists the Stepper Motor OPC UA exported APIs and features.
| Display Name | Valid Values |
|---|---|
| Stepper Motor Start (1111-Start) | Set the Motor Start value to 1111 to start the motor. The default is 0. |
| Stepper Motor Revolutions | Set the number of revolutions as follows:
|
| Stepper Motor Direction (0-Clockwise, 1-Anti-clockwise) | Set the Motor Direction value to 1 to run the motor in anti-clockwise direction. The default is 0 (Clockwise direction). |
| Stepper Motor Rotation (1-Full, 2-Half, and 3-Quarter) | Set the Motor Rotation value to 1|2|3 as required. By default, the stepper motor rotation is set to 1.
|
Important: The following example demonstrates the
procedure for sending OPC commands to the Stepper Motor:
- To start the stepper motor with
default values (Clockwise, Full Rotation), change the Stepper Motor
Start value from
0to1111. The stepper motor starts running in clockwise direction with the configured values. - To change the stepper motor
direction from clockwise to anti-clockwise direction, change the
Stepper Motor Direction value from
0to1. - To initiate 10 revolutions of the
stepper motor.
- Change the Stepper Motor
Revolutions value from
0to10. - Change the Stepper Motor
Start value from
0to1111. The stepper motor will start spinning in clockwise direction and should stop after 10 revolutions.
- Change the Stepper Motor
Revolutions value from