42.7.4 UHPHS USB Command Register
The Command Register indicates the command to be executed by the serial bus host controller. Writing to the register causes a command to be executed.
Name: | UHPHS_USBCMD |
Offset: | 0x10 |
Reset: | 0x00080B00 |
Property: | Read/Write |
Bit | 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | |
Access | |||||||||
Reset |
Bit | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | |
ITC[7:0] | |||||||||
Access | R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W | |
Reset | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 0 |
Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | |
ASPME | ASPMC[1:0] | ||||||||
Access | R-R/W | R-R/W | R-R/W | ||||||
Reset | 1 | 1 | 1 |
Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | |
LHCR | IAAD | ASE | PSE | FLS[1:0] | HCRESET | RS | |||
Access | R/W | R/W | R/W | R/W | R-R/W | R-R/W | R/W | R/W | |
Reset | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
Bits 23:16 – ITC[7:0] Interrupt Threshold Control
This field is used by system software to select the maximum rate at which the host controller will issue interrupts. The only valid values are defined below. If software writes an invalid value to this register, the results are undefined.
Value | Maximum Interrupt Interval |
---|---|
0 | Reserved |
1 | 1 microframe |
2 | 2 microframes |
4 | 4 microframes |
8 | 8 microframes (1 ms) |
16 | 16 microframes (2 ms) |
32 | 32 microframes (4 ms) |
64 | 64 microframes (8 ms) |
Any other value in this register yields undefined results.
Software modifications to this field while HCHLT=0 results in undefined behavior.
Bit 11 – ASPME Asynchronous Schedule Park Mode Enable (optional)
If the Asynchronous Park Capability bit in the UHPHS_HCCPARAMS register is set to 1, then this bit is set to 1 and is Read/Write. Otherwise the bit must be 0 and is read-only.
Value | Description |
---|---|
0 |
Park mode is enabled. |
1 |
Park mode is disabled. |
Bits 9:8 – ASPMC[1:0] Asynchronous Schedule Park Mode Count (optional)
If the Asynchronous Park Capability bit in the UHPHS_HCCPARAMS register is set to 1, then this field defaults to 3 and is read/write. Otherwise it defaults to 0 and is read-only. It contains a count of the number of successive transactions the host controller is allowed to execute from a high-speed queue head on the Asynchronous schedule before continuing traversal of the Asynchronous schedule. Valid values are 1 to 3. Software must not write a 0 to this bit when Park Mode Enable is set to 1 as this will result in undefined behavior.
Bit 7 – LHCR Light Host Controller Reset (optional)
This control bit is not required. If implemented, it allows the driver to reset the EHCI controller without affecting the state of the ports or the relationship to the companion host controllers. For example, the UHPHS_PORTSC registers should not be reset to their default values and the CF bit setting should not go to 0 (retaining port ownership relationships).
A host software read of this bit as 0 indicates the Light Host Controller Reset has completed and it is safe for host software to re-initialize the host controller. A host software read of this bit as 1 indicates the Light Host Controller Reset has not yet completed.
If not implemented, a read of this field will always return a 0.
Bit 6 – IAAD Interrupt on Async Advance Doorbell
This bit is used as a doorbell by software to tell the host controller to issue an interrupt the next time it advances asynchronous schedule. Software must write a 1 to this bit to ring the doorbell.
When the host controller has evicted all appropriate cached schedule state, it sets the Interrupt on Async Advance status bit in the UHPHS_USBSTS register. If the Interrupt on Async Advance Enable bit in the UHPHS_USBINTR register is set to 1, then the host controller will assert an interrupt at the next interrupt threshold.
The host controller sets this bit to 0 after it has set the Interrupt on Async Advance status bit in the UHPHS_USBSTS register to 1.
Software should not write a 1 to this bit when the asynchronous schedule is disabled. Doing so will yield undefined results.
Bit 5 – ASE Asynchronous Schedule Enable
This bit controls whether the host controller skips processing the Asynchronous Schedule.
Value | Description |
---|---|
0 | Do not process the Asynchronous Schedule. |
1 | Use the UHPHS_ASYNCLISTADDR register to access the Asynchronous Schedule. |
Bit 4 – PSE Periodic Schedule Enable
This bit controls whether the host controller skips processing the Periodic Schedule.
Value | Description |
---|---|
0 | Do not process the Periodic Schedule. |
1 | Use the UHPHS_PERIODICLISTBASE register to access the Periodic Schedule. |
Bits 3:2 – FLS[1:0] Frame List Size
This field is read-only with one exception: it is read/write if the Programmable Frame List flag, in the UHPHS_HCCPARAMS register, is set to 1. This field specifies the size of the frame list. The size of the frame list controls which bits in the Frame Index Register should be used for the Frame List Current index.
Value | Description |
---|---|
0 | 1024 elements (4096 bytes). |
1 | 512 elements (2048 bytes). |
2 | 256 elements (1024 bytes), for resource-constrained environments. |
3 | Reserved. |
Bit 1 – HCRESET Host Controller Reset
This control bit is used by software to reset the host controller. The effects of this on Root Hub registers are similar to a Chip Hardware Reset.
When software writes a 1 to this bit, the Host Controller resets its internal pipelines, timers, counters, state machines, etc. to their initial value. Any transaction currently in progress on USB is immediately terminated. A USB reset is not driven on downstream ports.
PCI Configuration registers are not affected by this reset. All operational registers, including port registers and port state machines, are set to their initial values. Port ownership reverts to the companion host controller(s) with side effects. Software must reinitialize the host controller in order to return the host controller to an operational state.
This bit is set to 0 by the Host Controller when the reset process is complete. Software cannot terminate the reset process early by writing a 0 to this register.
Software must not set this bit to 1 when HCHLT in the UHPHS_USBSTS register is 0. Attempting to reset an actively running host controller results in undefined behavior.
Bit 0 – RS Run/Stop
The Host Controller must halt within 16 microframes after software clears the bit RS. The HCHLT bit in the status register indicates when the Host Controller has finished its pending pipelined transactions and has entered the stopped state. Software must not write 1 to this field unless the host controller is in the halted state (i.e., HCHLT in the UHPHS_USBSTS register is 1). Doing so yields undefined results.
Value | Description |
---|---|
0 | Host Controller completes the current and any actively pipelined transactions on the USB and then halts. |
1 | Host Controller proceeds with execution of the schedule. |