24.4.4 Reset State Priorities
The reset state manager manages the following priorities between the different reset sources, given in descending order:
- Backup reset
- Wake-up reset
- Watchdog reset
- 32.768 kHz Crystal Oscillator Failure Detection reset
- Software reset
- User reset
Particular cases are listed below:
- When in user reset:
- A watchdog event is impossible because the watchdog timer is being reset by the processor reset signal.
- A software reset is impossible, since the processor reset is being activated.
- When in software reset:
- A watchdog event has priority over the current state.
- The NRST has no effect.
- When in watchdog reset:
- The processor reset is active and so a software reset cannot be programmed.
- A user reset cannot be entered.