Reversal of Write to Read
The host initiates the communication by a write command and finishes it by a read command. The figure below describes the REPEATED START and the reversal from Write mode to Read mode.
Note:
- In this case, if TWIHS_THR has not been written at the end of the read command, the clock is automatically stretched before the ACK.
- TXCOMP is only set at the end of the transmission. This is because after the REPEATED START, SADR is detected again.