1.3.3.23 SYS_NET_SetConfigParam Function

C

int32_t SYS_NET_SetConfigParam(SYS_MODULE_OBJ obj, uint32_t paramType, void *data)

Summary

Returns success on setting a configuration parameter for Net System Service.

Description

This function is currently used for enabling/ disabling the Auto Reconnect feature for the Net Socket.

Precondition

SYS_NET_Open should have been called.

Parameters

obj - SYS NET object handle, returned from SYS_NET_Open | Param | Description | |:----- |:----------- |

| paramType | Reserved for future use data - 0/ 1 currently used only for enabling/ disabling the auto reconnect feature

Returns

SYS_NET_SUCCESS - Indicates that the Request was catered to successfully

Example

bool auto_reconnect = true;
// Handle "objSysNet" value must have been returned from SYS_NET_Open.
if( SYS_NET_SetConfigParam(objSysNet, 0, &auto_reconnect) == SYS_NET_SUCCESS)
{
}

Remarks

None.