1.3.3.27 SYS_NET_GetStatus Function

C

SYS_NET_STATUS SYS_NET_GetStatus ( SYS_MODULE_OBJ object )

Summary

Returns System NET instance status.

Description

This function returns the current status of the System NET instance.

Precondition

SYS_NET_Open should have been called before calling this function

Parameters

ParamDescription
objectSYS NET object handle, returned from SYS_NET_Open

Returns

SYS_NET_STATUS

Example

// Handle "objSysNet" value must have been returned from SYS_NET_Open.
if (SYS_NET_GetStatus (objSysNet) == SYS_NET_STATUS_SERVER_AWAITING_CONNECTION)
{
    // NET system service is initialized and the NET server is ready to accept new connection.
}

Remarks

None.