1.3.3.30 SYS_NET_Task Function

C

void SYS_NET_Task(SYS_MODULE_OBJ obj)

Summary

Executes the SYS NET service state machine for the instance

Description

This function ensures that the Net system service is able to execute its state machine to process any messages and invoke the user callback for any events.

Precondition

SYS_NET_Open should have been called before calling this function

Parameters

ParamDescription
objSYS NET object handle, returned from SYS_NET_Open

Returns

None

Example

// Handle "objSysNet" value must have been returned from SYS_NET_Open.
while(1)
{
    ...
    SYS_NET_Task(objSysNet);
    ...
}