14.3 Block Diagram

The generation of Peripheral Clock signals (GCLK_PERIPHERAL) and the Main Clock (GCLK_MAIN) can be seen in the figure below.

Figure 14-1. Device Clocking Diagram

The GCLK block diagram is shown in the next figure.

Figure 14-2. Generic Clock Controller Block Diagram(1)
Note: 1. If GENCTRL.SRC=0x01(GCLKIN), the GCLK_IO is set as an input.