4.3.1 Mechanical Buttons
ATtiny3217 Xplained Pro contains two generic user-configurable mechanical buttons. When a button is pressed, it will drive the I/O line to GND.
Info: There is
no pull-up resistor connected to the generic user button SW0. Remember to enable the
internal pull-up in the ATtiny3217 to use
the button. There is an on-board pull-up resistor connected to the generic user button
SW1. There is no need to enable the internal pull-up in the ATtiny3217 to use the button.
| ATtiny3217 Pin | Silkscreen Text | Shared Functionality |
|---|---|---|
| PB5 | SW0 | EXT3 and EDBG DGI |
| PC5 | SW1/RST | EXT3 and UPDI debug connector |
Info: PC5 is
connected to a button that states 'SW1/RST' because PC5 had reset capabilities in an
early version of the ATtiny3217. Today the
ATtiny3217 does not have any reset
capabilities on PC5.