28.2.3.4 General Call Address Support
The addressing procedure for the I2C bus is such that the first byte after the Start condition usually determines which device will be the client addressed by the host device. The exception is the General Call address that can address all devices. When this address is used, all devices must, in theory, respond with an ACK.
The general call address is a reserved address in the I2C protocol, defined as address 0x00. When the General Call
Enable (GCEN) bit is set, the client module will automatically ACK the reception of this address regardless of the
value stored in SSPxADD. After the client clocks in an address of all zeros with the R/W bit clear, an interrupt is generated and
client software can read SSPxBUF and respond. Figure 28-14
shows a General Call reception sequence.
In 10-bit Address mode, the UA bit
will not be set on the reception of the general call address. The client will prepare to
receive the second byte as data, just as it would in 7-bit mode.