4.257.2 strtod.c
/* Copyright (c) 2002-2005 Michael Stumpf <mistumpf@de.pepperl-fuchs.com> Copyright (c) 2006,2008 Dmitry Xmelkov All rights reserved. Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met: * Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer. * Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution. * Neither the name of the copyright holders nor the names of contributors may be used to endorse or promote products derived from this software without specific prior written permission. THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /* $Id$ */ #if !defined(__AVR_TINY__) #include <avr/pgmspace.h> #include <ctype.h> #include <errno.h> #include <limits.h> #include <math.h> /* INFINITY, NAN */ #include <stdlib.h> #include "sectionname.h" /* Only GCC 4.2 calls the library function to convert an unsigned long to float. Other GCC-es (including 4.3) use a signed long to float conversion along with a large inline code to correct the result. */ extern double __floatunsisf (unsigned long); PROGMEM static const float pwr_p10 [6] = { 1e+1, 1e+2, 1e+4, 1e+8, 1e+16, 1e+32 }; PROGMEM static const float pwr_m10 [6] = { 1e-1, 1e-2, 1e-4, 1e-8, 1e-16, 1e-32 }; /* PSTR() is not used to save 1 byte per string: '\0' at the tail. */ PROGMEM static const char pstr_inf[] = {'I','N','F'}; PROGMEM static const char pstr_inity[] = {'I','N','I','T','Y'}; PROGMEM static const char pstr_nan[] = {'N','A','N'}; /** The strtod() function converts the initial portion of the string pointed to by \a nptr to double representation. The expected form of the string is an optional plus ( \c '+' ) or minus sign ( \c '-' ) followed by a sequence of digits optionally containing a decimal-point character, optionally followed by an exponent. An exponent consists of an \c 'E' or \c 'e', followed by an optional plus or minus sign, followed by a sequence of digits. Leading white-space characters in the string are skipped. The strtod() function returns the converted value, if any. If \a endptr is not \c NULL, a pointer to the character after the last character used in the conversion is stored in the location referenced by \a endptr. If no conversion is performed, zero is returned and the value of \a nptr is stored in the location referenced by \a endptr. If the correct value would cause overflow, plus or minus \c INFINITY is returned (according to the sign of the value), and \c ERANGE is stored in \c errno. If the correct value would cause underflow, zero is returned and \c ERANGE is stored in \c errno. */ ATTRIBUTE_CLIB_SECTION double strtod (const char * nptr, char ** endptr) { union { unsigned long u32; float flt; } x; unsigned char c; int exp; unsigned char flag; #define FL_MINUS 0x01 /* number is negative */ #define FL_ANY 0x02 /* any digit was readed */ #define FL_OVFL 0x04 /* overflow was */ #define FL_DOT 0x08 /* decimal '.' was */ #define FL_MEXP 0x10 /* exponent 'e' is neg. */ if (endptr) *endptr = (char *)nptr; do { c = *nptr++; } while (isspace (c)); flag = 0; if (c == '-') { flag = FL_MINUS; c = *nptr++; } else if (c == '+') { c = *nptr++; } if (!strncasecmp_P (nptr - 1, pstr_inf, 3)) { nptr += 2; if (!strncasecmp_P (nptr, pstr_inity, 5)) nptr += 5; if (endptr) *endptr = (char *)nptr; return flag & FL_MINUS ? -INFINITY : +INFINITY; } /* NAN() construction is not realised. Length would be 3 characters only. */ if (!strncasecmp_P (nptr - 1, pstr_nan, 3)) { if (endptr) *endptr = (char *)nptr + 2; return NAN; } x.u32 = 0; exp = 0; while (1) { c -= '0'; if (c <= 9) { flag |= FL_ANY; if (flag & FL_OVFL) { if (!(flag & FL_DOT)) exp += 1; } else { if (flag & FL_DOT) exp -= 1; /* x.u32 = x.u32 * 10 + c */ x.u32 = (((x.u32 << 2) + x.u32) << 1) + c; if (x.u32 >= (ULONG_MAX - 9) / 10) flag |= FL_OVFL; } } else if (c == (('.'-'0') & 0xff) && !(flag & FL_DOT)) { flag |= FL_DOT; } else { break; } c = *nptr++; } if (c == (('e'-'0') & 0xff) || c == (('E'-'0') & 0xff)) { int i; c = *nptr++; i = 2; if (c == '-') { flag |= FL_MEXP; c = *nptr++; } else if (c == '+') { c = *nptr++; } else { i = 1; } c -= '0'; if (c > 9) { nptr -= i; } else { i = 0; do { if (i < 3200) i = (((i << 2) + i) << 1) + c; /* i = 10*i + c */ c = *nptr++ - '0'; } while (c <= 9); if (flag & FL_MEXP) i = -i; exp += i; } } if ((flag & FL_ANY) && endptr) *endptr = (char *)nptr - 1; x.flt = __floatunsisf (x.u32); /* manually */ if ((flag & FL_MINUS) && (flag & FL_ANY)) x.flt = -x.flt; if (x.flt != 0) { int pwr; if (exp < 0) { nptr = (void *)(pwr_m10 + 5); exp = -exp; } else { nptr = (void *)(pwr_p10 + 5); } for (pwr = 32; pwr; pwr >>= 1) { for (; exp >= pwr; exp -= pwr) { union { unsigned long u32; float flt; } y; y.u32 = pgm_read_dword ((float *)nptr); x.flt *= y.flt; } nptr -= sizeof(float); } if (!isfinite(x.flt) || x.flt == 0) errno = ERANGE; } return x.flt; } #endif