2 <avr/io.h>: AVR device-specific IO definitions
This header file includes the apropriate IO definitions for the device that has
been specified by the -mmcu= compiler command-line switch. This is done by
diverting to the appropriate file <avr/ioXXXX.h>
which should never be included directly. Some register names common to all AVR devices are
defined directly within <avr/common.h>, which is included in
<avr/io.h>, but most of the details come from the
respective include file.
#include <avr/sfr_defs.h> #include <avr/portpins.h> #include <avr/common.h> #include <avr/version.h>See <avr/sfr_defs.h>: Special function registers for more details about that header file.
Included are definitions of the IO register set and their respective bit values as specified in the Atmel documentation. Note that inconsistencies in naming conventions, so even identical functions sometimes get different names on different devices.
Also included are the specific names useable for interrupt function definitions as documented here.
Finally, the following macros are defined:
-
RAMEND The last on-chip RAM address.
-
XRAMEND The last possible RAM location that is addressable. This is equal to RAMEND for devices that do not allow for external RAM. For devices that allow external RAM, this will be larger than RAMEND.
-
E2END The last EEPROM address.
-
FLASHEND The last byte address in the Flash program space.
-
SPM_PAGESIZE For devices with bootloader support, the flash pagesize (in bytes) to be used for the
SPMinstruction. -
E2PAGESIZE The size of the EEPROM page.