2 <util/delay.h>: Convenience functions for busy-wait delay loops
As an alternative method, it is possible to pass the F_CPU macro down to the compiler from the Makefile. Obviously, in that case, no #define statement should be used.
In order for these functions to work as intended, compiler optimizations must be enabled, and the delay time must be an expression that is a known constant at compile-time. If these requirements are not met, the resulting delay will be much longer (and basically unpredictable), and applications that otherwise do not use floating-point calculations will experience severe code bloat by the floating-point library routines linked into the application.