2 <avr/interrupt.h>: Interrupts
This discussion of interrupts was originally taken from Rich Neswold's document. See Acknowledgments.
It's nearly impossible to find compilers that agree on how to handle interrupt code. Since the C language tries to stay away from machine dependent details, each compiler writer is forced to design their method of support.
In the AVR-GCC environment, the vector table is predefined to point to interrupt routines with predetermined names. By using the appropriate name, your routine will be called when the corresponding interrupt occurs. The device library provides a set of default interrupt routines, which will get used if you don't define your own.
Patching into the vector table is only one part of the problem. The compiler
uses, by convention, a set of registers when it's normally executing compiler-generated code.
It's important that these registers, as well as the status register, get saved and restored.
The extra code needed to do this is enabled by tagging the interrupt function with
__attribute__((signal)).
These details seem to make interrupt routines a little messy, but all these details are handled by the Interrupt API. An interrupt routine is defined with ISR(). This macro register and mark the routine as an interrupt handler for the specified peripheral. The following is an example definition of a handler for the ADC interrupt.
Refer to the chapter explaining assembler programming for an explanation about interrupt routines written solely in assembler language.
Catch-all interrupt vector
If an unexpected interrupt occurs (interrupt is enabled and no handler is
installed, which usually indicates a bug), then the default action is to reset the device by
jumping to the reset vector. You can override this by supplying a function named
BADISR_vect which should be defined with ISR() as such. (The name BADISR_vect is actually an alias
for __vector_default. The latter must be used inside assembly code in case <avr/interrupt.h> is not included.)
Nested interrupts
The AVR hardware clears the global interrupt flag in SREG before entering an interrupt vector. Thus, normally interrupts will remain disabled inside the handler until the handler exits, where the RETI instruction (that is emitted by the compiler as part of the normal function epilogue for an interrupt handler) will eventually re-enable further interrupts. For that reason, interrupt handlers normally do not nest. For most interrupt handlers, this is the desired behaviour, for some it is even required in order to prevent infinitely recursive interrupts (like UART interrupts, or level-triggered external interrupts). In rare circumstances though it might be desired to re-enable the global interrupt flag as early as possible in the interrupt handler, in order to not defer any other interrupt more than absolutely needed. This could be done using an sei() instruction right at the beginning of the interrupt handler, but this still leaves few instructions inside the compiler-generated function prologue to run with global interrupts disabled. The compiler can be instructed to insert an SEI instruction right at the beginning of an interrupt handler by declaring the handler the following way:
ISR(XXX_vect, ISR_NOBLOCK) { ... }
where XXX_vect is the name of a valid interrupt vector for the
MCU type in question, as explained below.
Two vectors sharing the same code
In some circumstances, the actions to be taken upon two different interrupts might be completely identical so a single implementation for the ISR would suffice. For example, pin-change interrupts arriving from two different ports could logically signal an event that is independent from the actual port (and thus interrupt vector) where it happened. Sharing interrupt vector code can be accomplished using the ISR_ALIASOF() attribute to the ISR macro:
There is no body to the aliased ISR.
Empty interrupt service routines
In rare circumstances, in interrupt vector does not need any code to be implemented at all. The vector must be declared anyway, so when the interrupt triggers it won't execute the BADISR_vect code (which by default restarts the application).
This could for example be the case for interrupts that are solely enabled for the purpose of getting the controller out of sleep_mode().
A handler for such an interrupt vector can be declared using the EMPTY_INTERRUPT() macro:
There is no body to this macro.
In some circumstances, the compiler-generated prologue and epilogue of the ISR might not be optimal for the job, and a manually defined ISR could be considered particularly to speedup the interrupt handling.
One solution to this could be to implement the entire ISR as manual assembly code in a separate (assembly) file. See Combining C and assembly source files for an example of how to implement it that way.
Another solution is to still implement the ISR in C language but take over the
compiler's job of generating the prologue and epilogue. This can be done using the ISR_NAKED
attribute to the ISR() macro. Note that the compiler does not generate
anything as prologue or epilogue, so the final reti() must be provided by the actual implementation. SREG
must be manually saved if the ISR code modifies it, and the compiler-implied assumption of
__zero_reg__ always being 0 could be wrong (e. g. when interrupting right
after of a MUL instruction).
Choosing the vector: Interrupt vector names
The interrupt is chosen by supplying one of the symbols in following table.
There are currently two different styles present for naming the vectors. One
form uses names starting with SIG_, followed by a relatively verbose but
arbitrarily chosen name describing the interrupt vector. This has been the only available
style in avr-libc up to version 1.2.x.
Starting with avr-libc version 1.4.0, a second style of interrupt vector names
has been added, where a short phrase for the vector description is followed by
_vect. The short phrase matches the vector name as described in the
datasheet of the respective device (and in Atmel's XML files), with spaces replaced by an
underscore and other non-alphanumeric characters dropped. Using the suffix
_vect is intented to improve portability to other C compilers available for
the AVR that use a similar naming convention.
The historical naming style might become deprecated in a future release, so it is not recommended for new projects.
The ISR() macro cannot really spell-check the argument passed to them. Thus, by misspelling one of the names below in a call to ISR(), a function will be created that, while possibly being usable as an interrupt function, is not actually wired into the interrupt vector table. The compiler will generate a warning if it detects a suspiciously looking name of a ISR() function (i.e. one that after macro replacement does not start with "__vector_").
|
Vector name |
Old vector name |
Description |
Applicable for device |
|---|---|---|---|
|
ADC_vect |
SIG_ADC |
ADC Conversion Complete |
AT90S2333, AT90S4433, AT90S4434, AT90S8535, AT90PWM216, AT90PWM2B, AT90PWM316, AT90PWM3B, AT90PWM3, AT90PWM2, AT90PWM1, AT90CAN128, AT90CAN32, AT90CAN64, ATmega103, ATmega128, ATmega1284P, ATmega16, ATmega163, ATmega165, ATmega165P, ATmega168P, ATmega169, ATmega169P, ATmega32, ATmega323, ATmega325, ATmega3250, ATmega3250P, ATmega328P, ATmega329, ATmega3290, ATmega3290P, ATmega48P, ATmega64, ATmega645, ATmega6450, ATmega649, ATmega6490, ATmega8, ATmega8535, ATmega88P, ATmega168, ATmega48, ATmega88, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644, ATtiny13, ATtiny15, ATtiny26, ATtiny43U, ATtiny48, ATtiny24, ATtiny44, ATtiny84, ATtiny45, ATtiny25, ATtiny85, ATtiny261, ATtiny461, ATtiny861, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
ANALOG_COMP_0_vect |
SIG_COMPARATOR0 |
Analog Comparator 0 |
AT90PWM3, AT90PWM2, AT90PWM1 |
|
ANALOG_COMP_1_vect |
SIG_COMPARATOR1 |
Analog Comparator 1 |
AT90PWM3, AT90PWM2, AT90PWM1 |
|
ANALOG_COMP_2_vect |
SIG_COMPARATOR2 |
Analog Comparator 2 |
AT90PWM3, AT90PWM2, AT90PWM1 |
|
ANALOG_COMP_vect |
SIG_COMPARATOR |
Analog Comparator |
AT90CAN128, AT90CAN32, AT90CAN64, ATmega103, ATmega128, ATmega1284P, ATmega165, ATmega165P, ATmega168P, ATmega169, ATmega169P, ATmega325, ATmega3250, ATmega3250P, ATmega328P, ATmega329, ATmega3290, ATmega3290P, ATmega48P, ATmega64, ATmega645, ATmega6450, ATmega649, ATmega6490, ATmega88P, ATmega168, ATmega48, ATmega88, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644, AT90USB162, AT90USB82, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
ANA_COMP_vect |
SIG_COMPARATOR |
Analog Comparator |
AT90S1200, AT90S2313, AT90S2333, AT90S4414, AT90S4433, AT90S4434, AT90S8515, AT90S8535, ATmega16, ATmega161, ATmega162, ATmega163, ATmega32, ATmega323, ATmega8, ATmega8515, ATmega8535, ATtiny11, ATtiny12, ATtiny13, ATtiny15, ATtiny2313, ATtiny26, ATtiny28, ATtiny43U, ATtiny48, ATtiny24, ATtiny44, ATtiny84, ATtiny45, ATtiny25, ATtiny85, ATtiny261, ATtiny461, ATtiny861 |
|
CANIT_vect |
SIG_CAN_INTERRUPT1 |
CAN Transfer Complete or Error |
AT90CAN128, AT90CAN32, AT90CAN64 |
|
EEPROM_READY_vect |
SIG_EEPROM_READY, SIG_EE_READY |
ATtiny2313 | |
|
EE_RDY_vect |
SIG_EEPROM_READY |
EEPROM Ready |
AT90S2333, AT90S4433, AT90S4434, AT90S8535, ATmega16, ATmega161, ATmega162, ATmega163, ATmega32, ATmega323, ATmega8, ATmega8515, ATmega8535, ATtiny12, ATtiny13, ATtiny15, ATtiny26, ATtiny43U, ATtiny48, ATtiny24, ATtiny44, ATtiny84, ATtiny45, ATtiny25, ATtiny85, ATtiny261, ATtiny461, ATtiny861 |
|
EE_READY_vect |
SIG_EEPROM_READY |
EEPROM Ready |
AT90PWM3, AT90PWM2, AT90PWM1, AT90CAN128, AT90CAN32, AT90CAN64, ATmega103, ATmega128, ATmega1284P, ATmega165, ATmega165P, ATmega168P, ATmega169, ATmega169P, ATmega325, ATmega3250, ATmega3250P, ATmega328P, ATmega329, ATmega3290, ATmega3290P, ATmega32HVB, ATmega406, ATmega48P, ATmega64, ATmega645, ATmega6450, ATmega649, ATmega6490, ATmega88P, ATmega168, ATmega48, ATmega88, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644, ATmega16HVA, AT90USB162, AT90USB82, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
EXT_INT0_vect |
SIG_INTERRUPT0 |
External Interrupt Request 0 |
ATtiny24, ATtiny44, ATtiny84 |
|
INT0_vect |
SIG_INTERRUPT0 |
External Interrupt 0 |
AT90S1200, AT90S2313, AT90S2323, AT90S2333, AT90S2343, AT90S4414, AT90S4433, AT90S4434, AT90S8515, AT90S8535, AT90PWM216, AT90PWM2B, AT90PWM316, AT90PWM3B, AT90PWM3, AT90PWM2, AT90PWM1, AT90CAN128, AT90CAN32, AT90CAN64, ATmega103, ATmega128, ATmega1284P, ATmega16, ATmega161, ATmega162, ATmega163, ATmega165, ATmega165P, ATmega168P, ATmega169, ATmega169P, ATmega32, ATmega323, ATmega325, ATmega3250, ATmega3250P, ATmega328P, ATmega329, ATmega3290, ATmega3290P, ATmega32HVB, ATmega406, ATmega48P, ATmega64, ATmega645, ATmega6450, ATmega649, ATmega6490, ATmega8, ATmega8515, ATmega8535, ATmega88P, ATmega168, ATmega48, ATmega88, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644, ATmega16HVA, ATtiny11, ATtiny12, ATtiny13, ATtiny15, ATtiny22, ATtiny2313, ATtiny26, ATtiny28, ATtiny43U, ATtiny48, ATtiny45, ATtiny25, ATtiny85, ATtiny261, ATtiny461, ATtiny861, AT90USB162, AT90USB82, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
INT1_vect |
SIG_INTERRUPT1 |
External Interrupt Request 1 |
AT90S2313, AT90S2333, AT90S4414, AT90S4433, AT90S4434, AT90S8515, AT90S8535, AT90PWM216, AT90PWM2B, AT90PWM316, AT90PWM3B, AT90PWM3, AT90PWM2, AT90PWM1, AT90CAN128, AT90CAN32, AT90CAN64, ATmega103, ATmega128, ATmega1284P, ATmega16, ATmega161, ATmega162, ATmega163, ATmega168P, ATmega32, ATmega323, ATmega328P, ATmega32HVB, ATmega406, ATmega48P, ATmega64, ATmega8, ATmega8515, ATmega8535, ATmega88P, ATmega168, ATmega48, ATmega88, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644, ATmega16HVA, ATtiny2313, ATtiny28, ATtiny48, ATtiny261, ATtiny461, ATtiny861, AT90USB162, AT90USB82, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
INT2_vect |
SIG_INTERRUPT2 |
External Interrupt Request 2 |
AT90PWM3, AT90PWM2, AT90PWM1, AT90CAN128, AT90CAN32, AT90CAN64, ATmega103, ATmega128, ATmega1284P, ATmega16, ATmega161, ATmega162, ATmega32, ATmega323, ATmega32HVB, ATmega406, ATmega64, ATmega8515, ATmega8535, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644, ATmega16HVA, AT90USB162, AT90USB82, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
INT3_vect |
SIG_INTERRUPT3 |
External Interrupt Request 3 |
AT90PWM3, AT90PWM2, AT90PWM1, AT90CAN128, AT90CAN32, AT90CAN64, ATmega103, ATmega128, ATmega32HVB, ATmega406, ATmega64, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, AT90USB162, AT90USB82, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
INT4_vect |
SIG_INTERRUPT4 |
External Interrupt Request 4 |
AT90CAN128, AT90CAN32, AT90CAN64, ATmega103, ATmega128, ATmega64, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, AT90USB162, AT90USB82, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
INT5_vect |
SIG_INTERRUPT5 |
External Interrupt Request 5 |
AT90CAN128, AT90CAN32, AT90CAN64, ATmega103, ATmega128, ATmega64, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, AT90USB162, AT90USB82, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
INT6_vect |
SIG_INTERRUPT6 |
External Interrupt Request 6 |
AT90CAN128, AT90CAN32, AT90CAN64, ATmega103, ATmega128, ATmega64, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, AT90USB162, AT90USB82, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
INT7_vect |
SIG_INTERRUPT7 |
External Interrupt Request 7 |
AT90CAN128, AT90CAN32, AT90CAN64, ATmega103, ATmega128, ATmega64, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, AT90USB162, AT90USB82, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
IO_PINS_vect |
SIG_PIN, SIG_PIN_CHANGE |
External Interrupt Request 0 |
ATtiny11, ATtiny12, ATtiny15, ATtiny26 |
|
LCD_vect |
SIG_LCD |
LCD Start of Frame |
ATmega169, ATmega169P, ATmega329, ATmega3290, ATmega3290P, ATmega649, ATmega6490 |
|
LOWLEVEL_IO_PINS_vect |
SIG_PIN |
Low-level Input on Port B |
ATtiny28 |
|
OVRIT_vect |
SIG_CAN_OVERFLOW1 |
CAN Timer Overrun |
AT90CAN128, AT90CAN32, AT90CAN64 |
|
PCINT0_vect |
SIG_PIN_CHANGE0 |
Pin Change Interrupt Request 0 |
ATmega162, ATmega165, ATmega165P, ATmega168P, ATmega169, ATmega169P, ATmega325, ATmega3250, ATmega3250P, ATmega328P, ATmega329, ATmega3290, ATmega3290P, ATmega32HVB, ATmega406, ATmega48P, ATmega645, ATmega6450, ATmega649, ATmega6490, ATmega88P, ATmega168, ATmega48, ATmega88, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644, ATtiny13, ATtiny43U, ATtiny48, ATtiny24, ATtiny44, ATtiny84, ATtiny45, ATtiny25, ATtiny85, AT90USB162, AT90USB82, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
PCINT1_vect |
SIG_PIN_CHANGE1 |
Pin Change Interrupt Request 1 |
ATmega162, ATmega165, ATmega165P, ATmega168P, ATmega169, ATmega169P, ATmega325, ATmega3250, ATmega3250P, ATmega328P, ATmega329, ATmega3290, ATmega3290P, ATmega32HVB, ATmega406, ATmega48P, ATmega645, ATmega6450, ATmega649, ATmega6490, ATmega88P, ATmega168, ATmega48, ATmega88, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644, ATtiny43U, ATtiny48, ATtiny24, ATtiny44, ATtiny84, AT90USB162, AT90USB82 |
|
PCINT2_vect |
SIG_PIN_CHANGE2 |
Pin Change Interrupt Request 2 |
ATmega3250, ATmega3250P, ATmega328P, ATmega3290, ATmega3290P, ATmega48P, ATmega6450, ATmega6490, ATmega88P, ATmega168, ATmega48, ATmega88, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644, ATtiny48 |
|
PCINT3_vect |
SIG_PIN_CHANGE3 |
Pin Change Interrupt Request 3 |
ATmega3250, ATmega3250P, ATmega3290, ATmega3290P, ATmega6450, ATmega6490, ATmega324P, ATmega164P, ATmega644P, ATmega644, ATtiny48 |
|
PCINT_vect |
SIG_PIN_CHANGE, SIG_PCINT |
ATtiny2313, ATtiny261, ATtiny461, ATtiny861 | |
|
PSC0_CAPT_vect |
SIG_PSC0_CAPTURE |
PSC0 Capture Event |
AT90PWM3, AT90PWM2, AT90PWM1 |
|
PSC0_EC_vect |
SIG_PSC0_END_CYCLE |
PSC0 End Cycle |
AT90PWM3, AT90PWM2, AT90PWM1 |
|
PSC1_CAPT_vect |
SIG_PSC1_CAPTURE |
PSC1 Capture Event |
AT90PWM3, AT90PWM2, AT90PWM1 |
|
PSC1_EC_vect |
SIG_PSC1_END_CYCLE |
PSC1 End Cycle |
AT90PWM3, AT90PWM2, AT90PWM1 |
|
PSC2_CAPT_vect |
SIG_PSC2_CAPTURE |
PSC2 Capture Event |
AT90PWM3, AT90PWM2, AT90PWM1 |
|
PSC2_EC_vect |
SIG_PSC2_END_CYCLE |
PSC2 End Cycle |
AT90PWM3, AT90PWM2, AT90PWM1 |
|
SPI_STC_vect |
SIG_SPI |
Serial Transfer Complete |
AT90S2333, AT90S4414, AT90S4433, AT90S4434, AT90S8515, AT90S8535, AT90PWM216, AT90PWM2B, AT90PWM316, AT90PWM3B, AT90PWM3, AT90PWM2, AT90PWM1, AT90CAN128, AT90CAN32, AT90CAN64, ATmega103, ATmega128, ATmega1284P, ATmega16, ATmega161, ATmega162, ATmega163, ATmega165, ATmega165P, ATmega168P, ATmega169, ATmega169P, ATmega32, ATmega323, ATmega325, ATmega3250, ATmega3250P, ATmega328P, ATmega329, ATmega3290, ATmega3290P, ATmega32HVB, ATmega48P, ATmega64, ATmega645, ATmega6450, ATmega649, ATmega6490, ATmega8, ATmega8515, ATmega8535, ATmega88P, ATmega168, ATmega48, ATmega88, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644, ATmega16HVA, ATtiny48, AT90USB162, AT90USB82, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
SPM_RDY_vect |
SIG_SPM_READY |
Store Program Memory Ready |
ATmega16, ATmega162, ATmega32, ATmega323, ATmega8, ATmega8515, ATmega8535 |
|
SPM_READY_vect |
SIG_SPM_READY |
Store Program Memory Read |
AT90PWM3, AT90PWM2, AT90PWM1, AT90CAN128, AT90CAN32, AT90CAN64, ATmega128, ATmega1284P, ATmega165, ATmega165P, ATmega168P, ATmega169, ATmega169P, ATmega325, ATmega3250, ATmega3250P, ATmega328P, ATmega329, ATmega3290, ATmega3290P, ATmega406, ATmega48P, ATmega64, ATmega645, ATmega6450, ATmega649, ATmega6490, ATmega88P, ATmega168, ATmega48, ATmega88, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644, AT90USB162, AT90USB82, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
TIM0_COMPA_vect |
SIG_OUTPUT_COMPARE0A |
Timer/Counter Compare Match A |
ATtiny13, ATtiny43U, ATtiny24, ATtiny44, ATtiny84, ATtiny45, ATtiny25, ATtiny85 |
|
TIM0_COMPB_vect |
SIG_OUTPUT_COMPARE0B |
Timer/Counter Compare Match B |
ATtiny13, ATtiny43U, ATtiny24, ATtiny44, ATtiny84, ATtiny45, ATtiny25, ATtiny85 |
|
TIM0_OVF_vect |
SIG_OVERFLOW0 |
Timer/Counter0 Overflow |
ATtiny13, ATtiny43U, ATtiny24, ATtiny44, ATtiny84, ATtiny45, ATtiny25, ATtiny85 |
|
TIM1_CAPT_vect |
SIG_INPUT_CAPTURE1 |
Timer/Counter1 Capture Event |
ATtiny24, ATtiny44, ATtiny84 |
|
TIM1_COMPA_vect |
SIG_OUTPUT_COMPARE1A |
Timer/Counter1 Compare Match A |
ATtiny24, ATtiny44, ATtiny84, ATtiny45, ATtiny25, ATtiny85 |
|
TIM1_COMPB_vect |
SIG_OUTPUT_COMPARE1B |
Timer/Counter1 Compare Match B |
ATtiny24, ATtiny44, ATtiny84, ATtiny45, ATtiny25, ATtiny85 |
|
TIM1_OVF_vect |
SIG_OVERFLOW1 |
Timer/Counter1 Overflow |
ATtiny24, ATtiny44, ATtiny84, ATtiny45, ATtiny25, ATtiny85 |
|
TIMER0_CAPT_vect |
SIG_INPUT_CAPTURE0 |
ADC Conversion Complete |
ATtiny261, ATtiny461, ATtiny861 |
|
TIMER0_COMPA_vect |
SIG_OUTPUT_COMPARE0A |
TimerCounter0 Compare Match A |
ATmega168, ATmega48, ATmega88, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644, ATmega16HVA, ATtiny2313, ATtiny48, ATtiny261, ATtiny461, ATtiny861, AT90USB162, AT90USB82, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
TIMER0_COMPB_vect |
SIG_OUTPUT_COMPARE0B, SIG_OUTPUT_COMPARE0_B |
Timer Counter 0 Compare Match B |
AT90PWM3, AT90PWM2, AT90PWM1, ATmega1284P, ATmega168P, ATmega328P, ATmega32HVB, ATmega48P, ATmega88P, ATmega168, ATmega48, ATmega88, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644, ATmega16HVA, ATtiny2313, ATtiny48, ATtiny261, ATtiny461, ATtiny861, AT90USB162, AT90USB82, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
TIMER0_COMP_A_vect |
SIG_OUTPUT_COMPARE0A, SIG_OUTPUT_COMPARE0_A |
Timer/Counter0 Compare Match A |
AT90PWM3, AT90PWM2, AT90PWM1 |
|
TIMER0_COMP_vect |
SIG_OUTPUT_COMPARE0 |
Timer/Counter0 Compare Match |
AT90CAN128, AT90CAN32, AT90CAN64, ATmega103, ATmega128, ATmega16, ATmega161, ATmega162, ATmega165, ATmega165P, ATmega169, ATmega169P, ATmega32, ATmega323, ATmega325, ATmega3250, ATmega3250P, ATmega329, ATmega3290, ATmega3290P, ATmega64, ATmega645, ATmega6450, ATmega649, ATmega6490, ATmega8515, ATmega8535 |
|
TIMER0_OVF0_vect |
SIG_OVERFLOW0 |
Timer/Counter0 Overflow |
AT90S2313, AT90S2323, AT90S2343, ATtiny22, ATtiny26 |
|
TIMER0_OVF_vect |
SIG_OVERFLOW0 |
Timer/Counter0 Overflow |
AT90S1200, AT90S2333, AT90S4414, AT90S4433, AT90S4434, AT90S8515, AT90S8535, AT90PWM216, AT90PWM2B, AT90PWM316, AT90PWM3B, AT90PWM3, AT90PWM2, AT90PWM1, AT90CAN128, AT90CAN32, AT90CAN64, ATmega103, ATmega128, ATmega1284P, ATmega16, ATmega161, ATmega162, ATmega163, ATmega165, ATmega165P, ATmega168P, ATmega169, ATmega169P, ATmega32, ATmega323, ATmega325, ATmega3250, ATmega3250P, ATmega328P, ATmega329, ATmega3290, ATmega3290P, ATmega32HVB, ATmega48P, ATmega64, ATmega645, ATmega6450, ATmega649, ATmega6490, ATmega8, ATmega8515, ATmega8535, ATmega88P, ATmega168, ATmega48, ATmega88, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644, ATmega16HVA, ATtiny11, ATtiny12, ATtiny15, ATtiny2313, ATtiny28, ATtiny48, ATtiny261, ATtiny461, ATtiny861, AT90USB162, AT90USB82, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
TIMER1_CAPT1_vect |
SIG_INPUT_CAPTURE1 |
Timer/Counter1 Capture Event |
AT90S2313 |
|
TIMER1_CAPT_vect |
SIG_INPUT_CAPTURE1 |
Timer/Counter Capture Event |
AT90S2333, AT90S4414, AT90S4433, AT90S4434, AT90S8515, AT90S8535, AT90PWM216, AT90PWM2B, AT90PWM316, AT90PWM3B, AT90PWM3, AT90PWM2, AT90PWM1, AT90CAN128, AT90CAN32, AT90CAN64, ATmega103, ATmega128, ATmega1284P, ATmega16, ATmega161, ATmega162, ATmega163, ATmega165, ATmega165P, ATmega168P, ATmega169, ATmega169P, ATmega32, ATmega323, ATmega325, ATmega3250, ATmega3250P, ATmega328P, ATmega329, ATmega3290, ATmega3290P, ATmega48P, ATmega64, ATmega645, ATmega6450, ATmega649, ATmega6490, ATmega8, ATmega8515, ATmega8535, ATmega88P, ATmega168, ATmega48, ATmega88, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644, ATtiny2313, ATtiny48, AT90USB162, AT90USB82, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
TIMER1_CMPA_vect |
SIG_OUTPUT_COMPARE1A |
Timer/Counter1 Compare Match 1A |
ATtiny26 |
|
TIMER1_CMPB_vect |
SIG_OUTPUT_COMPARE1B |
Timer/Counter1 Compare Match 1B |
ATtiny26 |
|
TIMER1_COMP1_vect |
SIG_OUTPUT_COMPARE1A |
Timer/Counter1 Compare Match |
AT90S2313 |
|
TIMER1_COMPA_vect |
SIG_OUTPUT_COMPARE1A |
Timer/Counter1 Compare Match A |
AT90S4414, AT90S4434, AT90S8515, AT90S8535, AT90PWM216, AT90PWM2B, AT90PWM316, AT90PWM3B, AT90PWM3, AT90PWM2, AT90PWM1, AT90CAN128, AT90CAN32, AT90CAN64, ATmega103, ATmega128, ATmega1284P, ATmega16, ATmega161, ATmega162, ATmega163, ATmega165, ATmega165P, ATmega168P, ATmega169, ATmega169P, ATmega32, ATmega323, ATmega325, ATmega3250, ATmega3250P, ATmega328P, ATmega329, ATmega3290, ATmega3290P, ATmega32HVB, ATmega48P, ATmega64, ATmega645, ATmega6450, ATmega649, ATmega6490, ATmega8, ATmega8515, ATmega8535, ATmega88P, ATmega168, ATmega48, ATmega88, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644, ATmega16HVA, ATtiny2313, ATtiny48, ATtiny261, ATtiny461, ATtiny861, AT90USB162, AT90USB82, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
TIMER1_COMPB_vect |
SIG_OUTPUT_COMPARE1B |
Timer/Counter1 Compare MatchB |
AT90S4414, AT90S4434, AT90S8515, AT90S8535, AT90PWM216, AT90PWM2B, AT90PWM316, AT90PWM3B, AT90PWM3, AT90PWM2, AT90PWM1, AT90CAN128, AT90CAN32, AT90CAN64, ATmega103, ATmega128, ATmega1284P, ATmega16, ATmega161, ATmega162, ATmega163, ATmega165, ATmega165P, ATmega168P, ATmega169, ATmega169P, ATmega32, ATmega323, ATmega325, ATmega3250, ATmega3250P, ATmega328P, ATmega329, ATmega3290, ATmega3290P, ATmega32HVB, ATmega48P, ATmega64, ATmega645, ATmega6450, ATmega649, ATmega6490, ATmega8, ATmega8515, ATmega8535, ATmega88P, ATmega168, ATmega48, ATmega88, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644, ATmega16HVA, ATtiny2313, ATtiny48, ATtiny261, ATtiny461, ATtiny861, AT90USB162, AT90USB82, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
TIMER1_COMPC_vect |
SIG_OUTPUT_COMPARE1C |
Timer/Counter1 Compare Match C |
AT90CAN128, AT90CAN32, AT90CAN64, ATmega128, ATmega64, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, AT90USB162, AT90USB82, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
TIMER1_COMPD_vect |
SIG_OUTPUT_COMPARE0D |
Timer/Counter1 Compare Match D |
ATtiny261, ATtiny461, ATtiny861 |
|
TIMER1_COMP_vect |
SIG_OUTPUT_COMPARE1A |
Timer/Counter1 Compare Match |
AT90S2333, AT90S4433, ATtiny15 |
|
TIMER1_OVF1_vect |
SIG_OVERFLOW1 |
Timer/Counter1 Overflow |
AT90S2313, ATtiny26 |
|
TIMER1_OVF_vect |
SIG_OVERFLOW1 |
Timer/Counter1 Overflow |
AT90S2333, AT90S4414, AT90S4433, AT90S4434, AT90S8515, AT90S8535, AT90PWM216, AT90PWM2B, AT90PWM316, AT90PWM3B, AT90PWM3, AT90PWM2, AT90PWM1, AT90CAN128, AT90CAN32, AT90CAN64, ATmega103, ATmega128, ATmega1284P, ATmega16, ATmega161, ATmega162, ATmega163, ATmega165, ATmega165P, ATmega168P, ATmega169, ATmega169P, ATmega32, ATmega323, ATmega325, ATmega3250, ATmega3250P, ATmega328P, ATmega329, ATmega3290, ATmega3290P, ATmega32HVB, ATmega48P, ATmega64, ATmega645, ATmega6450, ATmega649, ATmega6490, ATmega8, ATmega8515, ATmega8535, ATmega88P, ATmega168, ATmega48, ATmega88, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644, ATmega16HVA, ATtiny15, ATtiny2313, ATtiny48, ATtiny261, ATtiny461, ATtiny861, AT90USB162, AT90USB82, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
TIMER2_COMPA_vect |
SIG_OUTPUT_COMPARE2A |
Timer/Counter2 Compare Match A |
ATmega168, ATmega48, ATmega88, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
TIMER2_COMPB_vect |
SIG_OUTPUT_COMPARE2B |
Timer/Counter2 Compare Match A |
ATmega168, ATmega48, ATmega88, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
TIMER2_COMP_vect |
SIG_OUTPUT_COMPARE2 |
Timer/Counter2 Compare Match |
AT90S4434, AT90S8535, AT90CAN128, AT90CAN32, AT90CAN64, ATmega103, ATmega128, ATmega16, ATmega161, ATmega162, ATmega163, ATmega165, ATmega165P, ATmega169, ATmega169P, ATmega32, ATmega323, ATmega325, ATmega3250, ATmega3250P, ATmega329, ATmega3290, ATmega3290P, ATmega64, ATmega645, ATmega6450, ATmega649, ATmega6490, ATmega8, ATmega8535 |
|
TIMER2_OVF_vect |
SIG_OVERFLOW2 |
Timer/Counter2 Overflow |
AT90S4434, AT90S8535, AT90CAN128, AT90CAN32, AT90CAN64, ATmega103, ATmega128, ATmega1284P, ATmega16, ATmega161, ATmega162, ATmega163, ATmega165, ATmega165P, ATmega168P, ATmega169, ATmega169P, ATmega32, ATmega323, ATmega325, ATmega3250, ATmega3250P, ATmega328P, ATmega329, ATmega3290, ATmega3290P, ATmega48P, ATmega64, ATmega645, ATmega6450, ATmega649, ATmega6490, ATmega8, ATmega8535, ATmega88P, ATmega168, ATmega48, ATmega88, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
TIMER3_CAPT_vect |
SIG_INPUT_CAPTURE3 |
Timer/Counter3 Capture Event |
AT90CAN128, AT90CAN32, AT90CAN64, ATmega128, ATmega1284P, ATmega162, ATmega64, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
TIMER3_COMPA_vect |
SIG_OUTPUT_COMPARE3A |
Timer/Counter3 Compare Match A |
AT90CAN128, AT90CAN32, AT90CAN64, ATmega128, ATmega1284P, ATmega162, ATmega64, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
TIMER3_COMPB_vect |
SIG_OUTPUT_COMPARE3B |
Timer/Counter3 Compare Match B |
AT90CAN128, AT90CAN32, AT90CAN64, ATmega128, ATmega1284P, ATmega162, ATmega64, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
TIMER3_COMPC_vect |
SIG_OUTPUT_COMPARE3C |
Timer/Counter3 Compare Match C |
AT90CAN128, AT90CAN32, AT90CAN64, ATmega128, ATmega64, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
TIMER3_OVF_vect |
SIG_OVERFLOW3 |
Timer/Counter3 Overflow |
AT90CAN128, AT90CAN32, AT90CAN64, ATmega128, ATmega1284P, ATmega162, ATmega64, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
TIMER4_CAPT_vect |
SIG_INPUT_CAPTURE4 |
Timer/Counter4 Capture Event |
ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561 |
|
TIMER4_COMPA_vect |
SIG_OUTPUT_COMPARE4A |
Timer/Counter4 Compare Match A |
ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561 |
|
TIMER4_COMPB_vect |
SIG_OUTPUT_COMPARE4B |
Timer/Counter4 Compare Match B |
ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561 |
|
TIMER4_COMPC_vect |
SIG_OUTPUT_COMPARE4C |
Timer/Counter4 Compare Match C |
ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561 |
|
TIMER4_OVF_vect |
SIG_OVERFLOW4 |
Timer/Counter4 Overflow |
ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561 |
|
TIMER5_CAPT_vect |
SIG_INPUT_CAPTURE5 |
Timer/Counter5 Capture Event |
ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561 |
|
TIMER5_COMPA_vect |
SIG_OUTPUT_COMPARE5A |
Timer/Counter5 Compare Match A |
ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561 |
|
TIMER5_COMPB_vect |
SIG_OUTPUT_COMPARE5B |
Timer/Counter5 Compare Match B |
ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561 |
|
TIMER5_COMPC_vect |
SIG_OUTPUT_COMPARE5C |
Timer/Counter5 Compare Match C |
ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561 |
|
TIMER5_OVF_vect |
SIG_OVERFLOW5 |
Timer/Counter5 Overflow |
ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561 |
|
TWI_vect |
SIG_2WIRE_SERIAL |
2-wire Serial Interface |
AT90CAN128, AT90CAN32, AT90CAN64, ATmega128, ATmega1284P, ATmega16, ATmega163, ATmega168P, ATmega32, ATmega323, ATmega328P, ATmega32HVB, ATmega406, ATmega48P, ATmega64, ATmega8, ATmega8535, ATmega88P, ATmega168, ATmega48, ATmega88, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644, ATtiny48, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
TXDONE_vect |
SIG_TXDONE |
Transmission Done, Bit Timer Flag 2 Interrupt |
AT86RF401 |
|
TXEMPTY_vect |
SIG_TXBE |
Transmit Buffer Empty, Bit Itmer Flag 0 Interrupt |
AT86RF401 |
|
UART0_RX_vect |
SIG_UART0_RECV |
UART0, Rx Complete |
ATmega161 |
|
UART0_TX_vect |
SIG_UART0_TRANS |
UART0, Tx Complete |
ATmega161 |
|
UART0_UDRE_vect |
SIG_UART0_DATA |
UART0 Data Register Empty |
ATmega161 |
|
UART1_RX_vect |
SIG_UART1_RECV |
UART1, Rx Complete |
ATmega161 |
|
UART1_TX_vect |
SIG_UART1_TRANS |
UART1, Tx Complete |
ATmega161 |
|
UART1_UDRE_vect |
SIG_UART1_DATA |
UART1 Data Register Empty |
ATmega161 |
|
UART_RX_vect |
SIG_UART_RECV |
UART, Rx Complete |
AT90S2313, AT90S2333, AT90S4414, AT90S4433, AT90S4434, AT90S8515, AT90S8535, ATmega103, ATmega163, ATmega8515 |
|
UART_TX_vect |
SIG_UART_TRANS |
UART, Tx Complete |
AT90S2313, AT90S2333, AT90S4414, AT90S4433, AT90S4434, AT90S8515, AT90S8535, ATmega103, ATmega163, ATmega8515 |
|
UART_UDRE_vect |
SIG_UART_DATA |
UART Data Register Empty |
AT90S2313, AT90S2333, AT90S4414, AT90S4433, AT90S4434, AT90S8515, AT90S8535, ATmega103, ATmega163, ATmega8515 |
|
USART0_RXC_vect |
SIG_USART0_RECV |
USART0, Rx Complete |
ATmega162 |
|
USART0_RX_vect |
SIG_UART0_RECV |
USART0, Rx Complete |
AT90CAN128, AT90CAN32, AT90CAN64, ATmega128, ATmega1284P, ATmega165, ATmega165P, ATmega169, ATmega169P, ATmega325, ATmega329, ATmega64, ATmega645, ATmega649, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644 |
|
USART0_TXC_vect |
SIG_USART0_TRANS |
USART0, Tx Complete |
ATmega162 |
|
USART0_TX_vect |
SIG_UART0_TRANS |
USART0, Tx Complete |
AT90CAN128, AT90CAN32, AT90CAN64, ATmega128, ATmega1284P, ATmega165, ATmega165P, ATmega169, ATmega169P, ATmega325, ATmega3250, ATmega3250P, ATmega329, ATmega3290, ATmega3290P, ATmega64, ATmega645, ATmega6450, ATmega649, ATmega6490, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644 |
|
USART0_UDRE_vect |
SIG_UART0_DATA |
USART0 Data Register Empty |
AT90CAN128, AT90CAN32, AT90CAN64, ATmega128, ATmega1284P, ATmega162, ATmega165, ATmega165P, ATmega169, ATmega169P, ATmega325, ATmega329, ATmega64, ATmega645, ATmega649, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644 |
|
USART1_RXC_vect |
SIG_USART1_RECV |
USART1, Rx Complete |
ATmega162 |
|
USART1_RX_vect |
SIG_UART1_RECV |
USART1, Rx Complete |
AT90CAN128, AT90CAN32, AT90CAN64, ATmega128, ATmega1284P, ATmega64, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644, AT90USB162, AT90USB82, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
USART1_TXC_vect |
SIG_USART1_TRANS |
USART1, Tx Complete |
ATmega162 |
|
USART1_TX_vect |
SIG_UART1_TRANS |
USART1, Tx Complete |
AT90CAN128, AT90CAN32, AT90CAN64, ATmega128, ATmega1284P, ATmega64, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644, AT90USB162, AT90USB82, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
USART1_UDRE_vect |
SIG_UART1_DATA |
USART1, Data Register Empty |
AT90CAN128, AT90CAN32, AT90CAN64, ATmega128, ATmega1284P, ATmega162, ATmega64, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644, AT90USB162, AT90USB82, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |
|
USART2_RX_vect |
SIG_USART2_RECV |
USART2, Rx Complete |
ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561 |
|
USART2_TX_vect |
SIG_USART2_TRANS |
USART2, Tx Complete |
ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561 |
|
USART2_UDRE_vect |
SIG_USART2_DATA |
USART2 Data register Empty |
ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561 |
|
USART3_RX_vect |
SIG_USART3_RECV |
USART3, Rx Complete |
ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561 |
|
USART3_TX_vect |
SIG_USART3_TRANS |
USART3, Tx Complete |
ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561 |
|
USART3_UDRE_vect |
SIG_USART3_DATA |
USART3 Data register Empty |
ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561 |
|
USART_RXC_vect |
SIG_USART_RECV, SIG_UART_RECV |
USART, Rx Complete |
ATmega16, ATmega32, ATmega323, ATmega8 |
|
USART_RX_vect |
SIG_USART_RECV, SIG_UART_RECV |
USART, Rx Complete |
AT90PWM3, AT90PWM2, AT90PWM1, ATmega168P, ATmega3250, ATmega3250P, ATmega328P, ATmega3290, ATmega3290P, ATmega48P, ATmega6450, ATmega6490, ATmega8535, ATmega88P, ATmega168, ATmega48, ATmega88, ATtiny2313 |
|
USART_TXC_vect |
SIG_USART_TRANS, SIG_UART_TRANS |
USART, Tx Complete |
ATmega16, ATmega32, ATmega323, ATmega8 |
|
USART_TX_vect |
SIG_USART_TRANS, SIG_UART_TRANS |
USART, Tx Complete |
AT90PWM3, AT90PWM2, AT90PWM1, ATmega168P, ATmega328P, ATmega48P, ATmega8535, ATmega88P, ATmega168, ATmega48, ATmega88, ATtiny2313 |
|
USART_UDRE_vect |
SIG_USART_DATA, SIG_UART_DATA |
USART Data Register Empty |
AT90PWM3, AT90PWM2, AT90PWM1, ATmega16, ATmega168P, ATmega32, ATmega323, ATmega3250, ATmega3250P, ATmega328P, ATmega3290, ATmega3290P, ATmega48P, ATmega6450, ATmega6490, ATmega8, ATmega8535, ATmega88P, ATmega168, ATmega48, ATmega88, ATtiny2313 |
|
USI_OVERFLOW_vect |
SIG_USI_OVERFLOW |
USI Overflow |
ATmega165, ATmega165P, ATmega169, ATmega169P, ATmega325, ATmega3250, ATmega3250P, ATmega329, ATmega3290, ATmega3290P, ATmega645, ATmega6450, ATmega649, ATmega6490, ATtiny2313 |
|
USI_OVF_vect |
SIG_USI_OVERFLOW |
USI Overflow |
ATtiny26, ATtiny43U, ATtiny24, ATtiny44, ATtiny84, ATtiny45, ATtiny25, ATtiny85, ATtiny261, ATtiny461, ATtiny861 |
|
USI_START_vect |
SIG_USI_START |
USI Start Condition |
ATmega165, ATmega165P, ATmega169, ATmega169P, ATmega325, ATmega3250, ATmega3250P, ATmega329, ATmega3290, ATmega3290P, ATmega645, ATmega6450, ATmega649, ATmega6490, ATtiny2313, ATtiny43U, ATtiny45, ATtiny25, ATtiny85, ATtiny261, ATtiny461, ATtiny861 |
|
USI_STRT_vect |
SIG_USI_START |
USI Start |
ATtiny26 |
|
USI_STR_vect |
SIG_USI_START |
USI START |
ATtiny24, ATtiny44, ATtiny84 |
|
WATCHDOG_vect |
SIG_WATCHDOG_TIMEOUT |
Watchdog Time-out |
ATtiny24, ATtiny44, ATtiny84 |
|
WDT_OVERFLOW_vect |
SIG_WATCHDOG_TIMEOUT, SIG_WDT_OVERFLOW |
Watchdog Timer Overflow |
ATtiny2313 |
|
WDT_vect |
SIG_WDT, SIG_WATCHDOG_TIMEOUT |
Watchdog Timeout Interrupt |
AT90PWM3, AT90PWM2, AT90PWM1, ATmega1284P, ATmega168P, ATmega328P, ATmega32HVB, ATmega406, ATmega48P, ATmega88P, ATmega168, ATmega48, ATmega88, ATmega640, ATmega1280, ATmega1281, ATmega2560, ATmega2561, ATmega324P, ATmega164P, ATmega644P, ATmega644, ATmega16HVA, ATtiny13, ATtiny43U, ATtiny48, ATtiny45, ATtiny25, ATtiny85, ATtiny261, ATtiny461, ATtiny861, AT90USB162, AT90USB82, AT90USB1287, AT90USB1286, AT90USB647, AT90USB646 |