4.34.10 deprecated.h
/* Copyright (c) 2005,2006 Joerg Wunsch
All rights reserved.
Redistribution and use in source and binary forms, with or without
modification, are permitted provided that the following conditions are met:
* Redistributions of source code must retain the above copyright
notice, this list of conditions and the following disclaimer.
* Redistributions in binary form must reproduce the above copyright
notice, this list of conditions and the following disclaimer in
the documentation and/or other materials provided with the
distribution.
* Neither the name of the copyright holders nor the names of
contributors may be used to endorse or promote products derived
from this software without specific prior written permission.
THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
POSSIBILITY OF SUCH DAMAGE. */
/* $Id$ */
#ifndef _COMPAT_DEPRECATED_H_
#define _COMPAT_DEPRECATED_H_
/** \defgroup deprecated_items <compat/deprecated.h>: Deprecated items
This header file contains several items that used to be available
in previous versions of this library, but have eventually been
deprecated over time.
\code #include <compat/deprecated.h> \endcode
These items are supplied within that header file for backward
compatibility reasons only, so old source code that has been
written for previous library versions could easily be maintained
until its end-of-life. Use of any of these items in new code is
strongly discouraged.
*/
/** \name Allowing specific system-wide interrupts
In addition to globally enabling interrupts, each device's particular
interrupt needs to be enabled separately if interrupts for this device are
desired. While some devices maintain their interrupt enable bit inside
the device's register set, external and timer interrupts have system-wide
configuration registers.
Example:
\code
// Enable timer 1 overflow interrupts.
timer_enable_int(_BV(TOIE1));
// Do some work...
// Disable all timer interrupts.
timer_enable_int(0);
\endcode
\note Be careful when you use these functions. If you already have a
different interrupt enabled, you could inadvertantly disable it by
enabling another intterupt. */
/*@{*/
/** \ingroup deprecated_items
\def enable_external_int(mask)
\deprecated
This macro gives access to the \c GIMSK register (or \c EIMSK register
if using an AVR Mega device or \c GICR register for others). Although this
macro is essentially the same as assigning to the register, it does
adapt slightly to the type of device being used. This macro is
unavailable if none of the registers listed above are defined. */
/* Define common register definition if available. */
#if defined(EIMSK)
# define __EICR EIMSK
#elif defined(GIMSK)
# define __EICR GIMSK
#elif defined(GICR)
# define __EICR GICR
#endif
/* If common register defined, define macro. */
#if defined(__EICR) || defined(__DOXYGEN__)
#define enable_external_int(mask) (__EICR = mask)
#endif
/** \ingroup deprecated_items
\deprecated
This function modifies the \c timsk register.
The value you pass via \c ints is device specific. */
static __inline__ void timer_enable_int (unsigned char ints)
{
#ifdef TIMSK
TIMSK = ints;
#endif
}
/** \def INTERRUPT(signame)
\ingroup deprecated_items
\deprecated
Introduces an interrupt handler function that runs with global interrupts
initially enabled. This allows interrupt handlers to be interrupted.
As this macro has been used by too many unsuspecting people in the
past, it has been deprecated, and will be removed in a future
version of the library. Users who want to legitimately re-enable
interrupts in their interrupt handlers as quickly as possible are
encouraged to explicitly declare their handlers as described
\ref attr_interrupt "above".
*/
#if (__GNUC__ == 4 && __GNUC_MINOR__ >= 1) || (__GNUC__ > 4)
# define __INTR_ATTRS used, externally_visible
#else /* GCC < 4.1 */
# define __INTR_ATTRS used
#endif
#ifdef __cplusplus
#define INTERRUPT(signame) \
extern "C" void signame(void); \
void signame (void) __attribute__ ((interrupt,__INTR_ATTRS)); \
void signame (void)
#else
#define INTERRUPT(signame) \
void signame (void) __attribute__ ((interrupt,__INTR_ATTRS)); \
void signame (void)
#endif
/*@}*/
/**
\name Obsolete IO macros
Back in a time when AVR-GCC and avr-libc could not handle IO port
access in the direct assignment form as they are handled now, all
IO port access had to be done through specific macros that
eventually resulted in inline assembly instructions performing the
desired action.
These macros became obsolete, as reading and writing IO ports can
be done by simply using the IO port name in an expression, and all
bit manipulation (including those on IO ports) can be done using
generic C bit manipulation operators.
The macros in this group simulate the historical behaviour. While
they are supposed to be applied to IO ports, the emulation actually
uses standard C methods, so they could be applied to arbitrary
memory locations as well.
*/
/*@{*/
/**
\ingroup deprecated_items
\def inp(port)
\deprecated
Read a value from an IO port \c port.
*/
#define inp(port) (port)
/**
\ingroup deprecated_items
\def outp(val, port)
\deprecated
Write \c val to IO port \c port.
*/
#define outp(val, port) (port) = (val)
/**
\ingroup deprecated_items
\def inb(port)
\deprecated
Read a value from an IO port \c port.
*/
#define inb(port) (port)
/**
\ingroup deprecated_items
\def outb(port, val)
\deprecated
Write \c val to IO port \c port.
*/
#define outb(port, val) (port) = (val)
/**
\ingroup deprecated_items
\def sbi(port, bit)
\deprecated
Set \c bit in IO port \c port.
*/
#define sbi(port, bit) (port) |= (1 << (bit))
/**
\ingroup deprecated_items
\def cbi(port, bit)
\deprecated
Clear \c bit in IO port \c port.
*/
#define cbi(port, bit) (port) &= ~(1 << (bit))
/*@}*/
#endif /* _COMPAT_DEPRECATED_H_ */