3.3.4 Zero-Crossing Detector Circuit
The phase identification is an important feature of the devices that are connected to Smart Grid networks, such as smart meters. A typical use of the zero-cross detection is to measure the time difference between a specific PLC frame reception and the last zero crossing event of the mains single-phase to which the device is connected.
The Figure 3-14 shows the Zero-Crossing Detection circuit used in the PL460-EK board, which features detection of rising edges of the mains voltage. The output signal of the detection circuit, Zero-crossing Detector, is connected to the VZC pin of the PL460, and a synchronization algorithm is applied to obtain an accurate measurement of the time between the reception of a PLC frame and the zero-crossing event.