6.2.2 Firmware is Already Downloaded
If the firmware is already downloaded, the host can perform the following:
- Change the UART parameters like the baud rate and flow control options
- Change the BD address of the Bluetooth controller if the BD address is not stored on the controller
- Send a Reset command. This is mandatory if the BD address is changed