2.1 The device does not boot on some QSPI memories

A bug in the ROM code can prevent toggling some QSPI memory models in Quad SPI mode (1-4-4) before issuing a (1-4-4) fast read quad I/O command. As a result, booting is not possible using these memories.

Work Around

Use a memory with Quad mode enabled by default (for example, using an SST26VF064BA model instead of an SST26VF064B model).

Affected Device Revisions

A0

A0-D1G

A0-D2G

A1

A1-D5M

A1-D1G

A1-D2G

A2

A2-D5M

A2-D1G

A2-D2G

X––