15.3.2.3 Event Generators
Each event channel has several possible event generators, but only one can be selected at a time. The event generator for a channel is selected by writing to the respective Channel n Generator Selection (EVSYS.CHANNELn) register. By default, the channels are not connected to any event generator. For details on event generation, refer to the documentation of the corresponding peripheral.
A generated event is either synchronous or asynchronous to the device peripheral clock (CLK_PER). Asynchronous events can be generated outside the normal edges of the peripheral clock, making the system respond faster than the selected clock frequency would suggest. Asynchronous events can also be generated while the device is in a sleep mode when the peripheral clock is not running.
Any generated event is classified as either a pulse event or a level event. In both cases, the event can be either synchronous or asynchronous, with properties according to the table below.
| Event Type | Sync/Async | Description |
|---|---|---|
| Pulse | Sync | An event generated from CLK_PER that lasts one clock cycle |
| Async | An event generated from a clock other than CLK_PER lasting one clock cycle | |
| Level | Sync | An event generated from CLK_PER that lasts multiple clock cycles |
| Async | An event generated without a clock (for example, a pin or a comparator), or an event generated from a clock other than CLK_PER that lasts multiple clock cycles |
The properties of both the generated event and the intended event user must be considered in order to ensure reliable and predictable operation.
The table below shows the available event generators for this device family.
| Generator Name | Description | Event Type | Generating Clock Domain | Length of event | |||
|---|---|---|---|---|---|---|---|
| Peripheral | Event | ||||||
| UPDI | SYNCH | SYNCH character | Level | CLK_PDI | SYNCH character on PDI RX input synchronized to CLK_PDI | ||
| RTC | OVF | Overflow | Pulse | CLK_RTC | One CLK_RTC period | ||
| CMP | Compare Match | ||||||
| PIT_DIV8192 | Prescaled RTC clock divided by 8192 | Level | Given by prescaled RTC clock divided by 8192 | ||||
| PIT_DIV4096 | Prescaled RTC clock divided by 4096 | Given by prescaled RTC clock divided by 4096 | |||||
| PIT_DIV2048 | Prescaled RTC clock divided by 2048 | Given by prescaled RTC clock divided by 2048 | |||||
| PIT_DIV1024 | Prescaled RTC clock divided by 1024 | Given by prescaled RTC clock divided by 1024 | |||||
| PIT_DIV512 | Prescaled RTC clock divided by 512 | Given by prescaled RTC clock divided by 512 | |||||
| PIT_DIV256 | Prescaled RTC clock divided by 256 | Given by prescaled RTC clock divided by 256 | |||||
| PIT_DIV128 | Prescaled RTC clock divided by 128 | Given by prescaled RTC clock divided by 128 | |||||
| PIT_DIV64 | Prescaled RTC clock divided by 64 | Given by prescaled RTC clock divided by 64 | |||||
| CCL | LUTn | LUT output level | Level | Asynchronous | Depends on CCL configuration | ||
| ACn | OUT | Comparator output level | Level | Asynchronous | Given by AC output level | ||
| ADCn | RESRDY | Result ready | Pulse | CLK_PER | One CLK_PER period | ||
| PTC | RESRDY | Result ready | Pulse | CLK_PER | One CLK_PER period | ||
| ZCDn | OUT | ZCD output level | Level | Asynchronous | Given by ZCD output level | ||
| PORTx | PINn | Pin level | Level | Asynchronous | Given by pin level | ||
| USARTn | XCK | USART Baud clock | Level | CLK_PER | Minimum two CLK_PER periods | ||
| SPIn | SCK | SPI Host clock | Level | CLK_PER | Minimum two CLK_PER periods | ||
| TCAn | OVF_LUNF | Overflow/Low byte timer underflow | Pulse | CLK_PER | One CLK_PER period | ||
| HUNF | High byte timer underflow | ||||||
| CMP0_LCMP0 | Compare channel 0 match/Low byte timer compare channel 0 match | ||||||
| CMP1_LCMP1 | Compare channel 1 match/Low byte timer compare channel 1 match | ||||||
| CMP2_LCMP2 | Compare channel 2 match/Low byte timer compare channel 2 match | ||||||
| TCBn | CAPT | CAPT flag set | Pulse | CLK_PER | One CLK_PER period | ||
| OVF | Overflow | ||||||
| TCDn | CMPBCLR | Counter matches CMPBCLR | Pulse | CLK_TCD | One CLK_TCD period | ||
| CMPASET | Counter matches CMPASET | ||||||
| CMPBSET | Counter matches CMPBSET | ||||||
| PROGEV | Programmable event output | ||||||