6.7 Battery Charging
The IS2083BM SoC has a built-in battery charger that is optimized for lithium-ion and lithium polymer batteries.
The on-chip PMU integrates the battery charger and voltage regulator. A power switch is used to switch over the power source between the battery (BAT_IN) and an adapter (ADAP_IN). The PMU provides the current to drive two LEDs.
The battery charger supports various modes with the features listed below:
- Charging control using current sensor
- User-programmable current regulation
- High accuracy voltage regulation
- Constant current and constant voltage modes
- Stop charging and re-charging modes
The following figure illustrates the charging curve of a battery.
Note: For more details on battery charger configuration, please refer to the IS2083/BM83
Battery Charger Application Note (AN3490).