1.29.27.2 TCCx_Timer16bitCompareSet Function
C
/* x = TCC instance number */ void TCCx_Timer16bitCompareSet ( uint16_t compare );
Summary
Sets the compare value of a given timer channel.
Description
This function writes the compare value. When timer counter matches compare value, interrupt can be generated.
Precondition
TCCx_TimerInitialize function must have been called first for the given channel.
Parameters
Param | Description |
---|---|
compare | compare value of the timer |
Returns
None.
Example
TCC0_TimerInitialize();
TCC0_Timer16bitCompareSet(0xFul);
Remarks
This function is available only when TCC timer mode is used by SYS_TIME module. SYS_TIME uses compare match interrupt to generate dynamic delay.