1.24.1.17 ADCHS_DMASampleCountBaseAddrSet Function
C
void ADCHS_DMASampleCountBaseAddrSet(uint32_t baseAddr)
Summary
Registers the user-defined RAM address at which the DMA engine will start saving the current count of output samples
Description
Registers the user-defined RAM address at which the DMA engine will start saving the current count of output samples
Precondition
ADCHS_Initialize() must have been called first for the associated instance.
Parameters
Param | Description |
---|---|
baseAddr | Physical address of the user-defined RAM address |
Returns
None.
Example
__COHERENT uint8_t adcSampleCntBuffer; ADCHS_DMASampleCountBaseAddrSet((uint32_t)KVA_TO_PA(adcSampleCntBuffer));
Remarks
None