1.26.8.2 OTPC_WritePacket Function

C

otpc_error_code_t OTPC_WritePacket(const OTPC_NEW_PACKET *packet,
const uint32_t *payload,
uint16_t *headerAddress,
uint16_t *sizeWritten);

Summary

Perform an OTPC packet write.

Description

Create a new packet with the given payload. Returns the address of the packet and size written (in number of bytes).

Precondition

OTPC_Initialize() function must have been called first.

Parameters

Param Description
packet Pointer to the structure defining the packet attributes
payload Pointer to the address of new payload
headerAddress Address of the newly created packet(output)}
sizeWritten number of bytes written into the new packet

Returns

otpc error code.

Example

OTPC_Initialize();
OTPC_WritePacket(&packet, &payload, &headerAddress, &sizeWritten);

Remarks

None