1.26.4 Debug Unit (DBGU)

The DBGU peripheral library (PLIB) can be configured either in blocking (interrupt disabled), non-blocking (interrupt enabled) or ring buffer mode.

Blocking mode

In blocking mode, the DBGU peripheral interrupts are disabled and the transfer APIs block until the requested data is transferred.

Non-blocking mode

In non-blocking mode the peripheral interrupt is enabled. The transfer API initiates the transfer and returns immediately. The transfer is then completed from the peripheral interrupt. Application can either use a callback to get notified when the transfer is complete or can use the IsBusy API to check the completion status.

Ring buffer mode

In ring buffer mode, the receiver is always enabled, and the received data is saved in the internal receive ring buffer, size of which can be configured using MHC. The application can use the API calls to read the data out from the ring buffer. APIs are provided to query the number of (unread) bytes available in the receive buffer, free space in the receive buffer and size of the receive buffer. Similarly, during transmission, the application data is deep copied into the internal transmit ring buffer, size of which can be configured using MHC. This allows the use of local buffers for data transmission. APIs are provided to query the free space in the transmit buffer, number of bytes pending transmission and the size of the transmit buffer. Additionally, application can enable notifications to get notified when n bytes are available in the receive buffer or when n bytes of free space is available in the transmit buffer. The APIs allow application to set the threshold levels for notification in both receive and transmit buffers. Further, application can also choose to enable persistent notifications, whereby the application is notified until the threshold condition is met.

In all the modes, library provides API to change the baud, parity, data width and the number of stop bits at run time.

Using The Library

Blocking Mode

#define RX_BUFFER_SIZE 10
char message[] = "DBGU Example in blocking mode";
char receiveBuffer[RX_BUFFER_SIZE] = {0};
DBGU_ERROR errorStatus;
char rxData = 0;

int main ( void )
{    
    /* Initialize all modules */
    SYS_Initialize ( NULL );

    /* Transmit buffer*/
    DBGU_Write(message, sizeof(message));
	
	/* Wait for a character to be received */
	while(DBGU_ReceiverIsReady() == false);
		
	if(DBGU_ErrorGet() == DBGU_ERROR_NONE)
	{
		/* Read a byte */
		rxData = DBGU_ReadByte();
	}
	
	/* Receive buffer */
    if (DBGU_Read(receiveBuffer, RX_BUFFER_SIZE)) == false)
	{
		/* Read failed, get the error */
		errorStatus DBGU_ErrorGet();
		
		/* Handle the error */
	}
    else
	{
		/* Transmit the received buffer*/
		DBGU_Write(receiveBuffer, RX_BUFFER_SIZE);
	}

	...

    /* Execution should not come here during normal operation */

    return ( EXIT_FAILURE );
}

Non-blocking Mode

#define RX_BUFFER_SIZE 10

char message[] = "**** Non-blocking Transfer with the interrupt  ****\r\n\
**** Type 10 characters. The received characters are echoed back ****\r\n";

char messageError[] = "**** DBGU error occurred ****\r\n";

char receiveBuffer[RX_BUFFER_SIZE] = {0};
char echoBuffer[RX_BUFFER_SIZE+4] = {0};

bool errorStatus = false;
bool writeStatus = false;
bool readStatus = false;

void APP_WriteCallback(uintptr_t context)
{
    writeStatus = true;
}

void APP_ReadCallback(uintptr_t context)
{
    if(DBGU_ErrorGet() != DBGU_ERROR_NONE)
    {
        /* ErrorGet clears errors, set error flag to notify console */
        errorStatus = true;
    }
    else
    {
        readStatus = true;
    }
}

int main ( void )
{
    /* Initialize all modules */
    SYS_Initialize ( NULL );

    /* Register callback functions and send start message */
    DBGU_WriteCallbackRegister(APP_WriteCallback, 0);
    DBGU_ReadCallbackRegister(APP_ReadCallback, 0);
    DBGU_Write(&message[0], sizeof(message));

    while ( true )
    {
        if(errorStatus == true)
        {
            /* Send error message to console */
            errorStatus = false;
            DBGU_Write(&messageError[0], sizeof(messageError));
        }
        else if(readStatus == true)
        {
            /* Echo back received buffer and Toggle LED */
            readStatus = false;

            echoBuffer[0] = '\n';
            echoBuffer[1] = '\r';
            memcpy(&echoBuffer[2], receiveBuffer,sizeof(receiveBuffer));
            echoBuffer[RX_BUFFER_SIZE+2] = '\n';
            echoBuffer[RX_BUFFER_SIZE+3] = '\r';

            DBGU_Write(&echoBuffer[0], sizeof(echoBuffer));
        }
        else if(writeStatus == true)
        {
            /* Submit buffer to read user data */
            writeStatus = false;
            DBGU_Read(&receiveBuffer[0], sizeof(receiveBuffer));
        }
        else
        {
            /* Repeat the loop */
            ;
        }
    }

    /* Execution should not come here during normal operation */

    return ( EXIT_FAILURE );
}

Ring buffer Mode

uint8_t txBuffer[50];
uint8_t rxBuffer[10];
volatile uint32_t nBytesRead = 0;
volatile bool txThresholdEventReceived = false;
volatile bool rxThresholdEventReceived = false;

void DBGUReadEventHandler(DBGU_EVENT event, uintptr_t context )
{
    uint32_t nBytesAvailable = 0;
    
    if (event == DBGU_EVENT_READ_THRESHOLD_REACHED)
    {
        /* Receiver should atleast have the thershold number of bytes in the ring buffer */
        nBytesAvailable = DBGU_ReadCountGet();
        
        nBytesRead += DBGU_Read((uint8_t*)&rxBuffer[nBytesRead], nBytesAvailable);                          
    }
}

void DBGUWriteEventHandler(DBGU_EVENT event, uintptr_t context )
{
    txThresholdEventReceived = true;
}

int main ( void )
{
    uint32_t nBytes = 0;        
    
    /* Initialize all modules */
    SYS_Initialize ( NULL );          
    
    /* Register a callback for write events */
    DBGU_WriteCallbackRegister(DBGUWriteEventHandler, (uintptr_t) NULL);
    
    /* Register a callback for read events */
    DBGU_ReadCallbackRegister(DBGUReadEventHandler, (uintptr_t) NULL);              
    
    /* Print the size of the read buffer on the terminal */
    nBytes = sprintf((char*)txBuffer, "RX Buffer Size = %d\r\n", (int)DBGU_ReadBufferSizeGet());
    
    DBGU_Write((uint8_t*)txBuffer, nBytes);  
    
    /* Print the size of the write buffer on the terminal */
    nBytes = sprintf((char*)txBuffer, "TX Buffer Size = %d\r\n", (int)DBGU_WriteBufferSizeGet());
    
    DBGU_Write((uint8_t*)txBuffer, nBytes);    
    
    DBGU_Write((uint8_t*)"Adding 10 characters to the TX buffer - ", sizeof("Adding 10 characters to the TX buffer - "));    
    
    /* Wait for all bytes to be transmitted out */
    while (DBGU_WriteCountGet() != 0);    
    
    DBGU_Write((uint8_t*)"0123456789", 10);           
        
    /* Print the amount of free space available in the TX buffer. This should be 10 bytes less than the configured write buffer size. */
    nBytes = sprintf((char*)txBuffer, "\r\nFree Space in Transmit Buffer = %d\r\n", (int)DBGU_WriteFreeBufferCountGet());

    DBGU_Write((uint8_t*)txBuffer, nBytes);    
    
    /* Let's enable notifications to get notified when the TX buffer is empty */
    DBGU_WriteThresholdSet(DBGU_WriteBufferSizeGet());   
    
    /* Enable notifications */
    DBGU_WriteNotificationEnable(true, false);
   
    /* Wait for the TX buffer to become empty. Flag "txThresholdEventReceived" is set in the callback. */
    while (txThresholdEventReceived == false);
    
    txThresholdEventReceived = false;    
    
    /* Disable TX notifications */
    DBGU_WriteNotificationEnable(false, false);
    
    DBGU_Write((uint8_t*)"Enter 10 characters. The received characters are echoed back. \r\n>", sizeof("Enter 10 characters. The received characters are echoed back. \r\n>"));               
            
    /* Wait till 10 (or more) characters are received */
    while (DBGU_ReadCountGet() < 10);
    
    /* At-least 10 characters are available in the RX buffer. Read out into the application buffer */
    DBGU_Read((uint8_t*)rxBuffer, 10);  
    
    /* Echo the received data */
    DBGU_Write((uint8_t*)rxBuffer, 10);    
    
    /* Now demonstrating receiver notifications */
    DBGU_Write((uint8_t*)"\r\n Now turning on RX notifications \r\n>", sizeof("\r\n Now turning on RX notifications \r\n>"));
    
    /* For demonstration purpose, set a threshold value to receive a callback after every 5 characters are received */
    DBGU_ReadThresholdSet(5);
    
    /* Enable RX event notifications */
    DBGU_ReadNotificationEnable(true, false);
                   
    while(1)
    {
        /* Wait until at-least 10 characters are entered by the user */
        while (nBytesRead < 10);    
    
        /* Echo the received data */
        DBGU_Write((uint8_t*)rxBuffer, nBytesRead);
        
        DBGU_Write((uint8_t*)"\r\n>", 3);

        nBytesRead = 0;
    }

    /* Execution should not come here during normal operation */

    return ( EXIT_FAILURE );
}

Library Interface

DBGU peripheral library provides the following interfaces:

Functions

Name Description Blocking mode Non-blocking mode Ring buffer mode
DBGU_Initialize Initializes given instance of the DBGU peripheral Yes Yes Yes
DBGU_SerialSetup Sets up serial configurations for DBGU peripheral Yes Yes Yes
DBGU_Write Writes data to the given DBGU peripheral instance Yes Yes Yes
DBGU_Read Reads data from the given DBGU peripheral instance Yes Yes Yes
DBGU_WriteIsBusy Returns the write request status associated with the given DBGU peripheral instance No Yes No
DBGU_ReadIsBusy Returns the read request status associated with the given DBGU peripheral instance No Yes No
DBGU_WriteCountGet Gets the byte count of processed bytes for a given DBGU read operation in non-blocking mode. Returns the number of bytes pending to be transmitted out in the transmit buffer in ring buffer mode. No Yes Yes
DBGU_ReadCountGet Gets the byte count of processed bytes for a given DBGU read operation in non-blocking mode. Returns the number of bytes available in the internal receive buffer of the PLIB in ring buffer mode. No Yes Yes
DBGU_TransmitterIsReady Returns the hardware status of the DBGU Transmitter Yes No No
DBGU_ReceiverIsReady Returns the hardware status of the DBGU Receiver Yes No No
DBGU_ErrorGet Gets the error of the given DBGU peripheral instance Yes Yes Yes
DBGU_WriteCallbackRegister Sets the pointer to the function (and it's context) to be called when the given DBGU's write events occur No Yes Yes
DBGU_ReadCallbackRegister Sets the pointer to the function (and it's context) to be called when the given DBGU's read events occur No Yes Yes
DBGU_ReadByte Submits request to read a byte of data to the given DBGU peripheral Yes No No
DBGU_WriteByte Submits a byte of data to the given DBGU peripheral to transfer Yes No No
DBGU_ReadAbort Aborts the ongoing read request No Yes No
DBGU_WriteFreeBufferCountGet Returns the number of bytes of free space available in the internal transmit buffer No No Yes
DBGU_WriteBufferSizeGet Returns the size of the internal transmit ring buffer No No Yes
DBGU_WriteNotificationEnable This API lets the application turn the transmit notifications on/off No No Yes
DBGU_WriteThresholdSet This API allows the application to set a threshold level on the number of free space available in the transmit buffer No No Yes
DBGU_ReadFreeBufferCountGet Returns the number of bytes of free space available in the internal receive buffer No No Yes
DBGU_ReadBufferSizeGet Returns the size of the receive ring buffer No No Yes
DBGU_ReadNotificationEnable This API lets the application turn the receive notifications on/off No No Yes
DBGU_ReadThresholdSet This API allows the application to set a threshold level on the number of bytes of data available in the receive buffer No No Yes

Data types and constants

Name Type Description Blocking mode Non-blocking mode Ring buffer mode
DBGU_ERROR Macros and Typedef Defines the macros and typedefs associated with the DBGU peripheral errors Yes Yes Yes
DBGU_PARITY Enum Defines the parity types for the DBGU peripheral Yes Yes Yes
DBGU_SERIAL_SETUP Struct Defines the data structure which is used to configure DBGU serial parameters at run time Yes Yes Yes
DBGU_CALLBACK Typedef Defines the data type and function signature of the DBGU peripheral library callback function Yes Yes No
DBGU_EVENT Enum Defines the enums associated with the DBGU events in the ring buffer mode Yes Yes Yes
DBGU_RING_BUFFER_CALLBACK Typedef Defines the data type and function signature for the DBGU peripheral callback function in the ring buffer mode No No Yes