1.21.2.14 CANx_TxFIFOIsFull Function
C
bool CANx_TxFIFOIsFull(uint8_t fifoNum) // x - Instance of the CAN peripheral
Summary
Returns true if Tx FIFO is full otherwise false.
Description
This routine returns true if Tx FIFO is full otherwise false.
Precondition
CANx_Initialize must have been called for the associated CAN instance.
Parameters
Param | Description |
---|---|
fifoNum | FIFO number |
Returns
true - Tx FIFO is full.
false - Tx FIFO is not full.
Example
if (CAN0_TxFIFOIsFull(1) == false)
{
// Tx FIFO is not full
}
Remarks
None.