1.25.6.76 FLEXCOM_TWI_CALLBACK Typedef
C
/* TWI master mode */ typedef void (*FLEXCOM_TWI_CALLBACK) (uintptr_t contextHandle)
Summary
Defines the data type and function signature for the FLEXCOM TWI peripheral callback function in TWI master mode.
Description
This data type defines the function signature for the FLEXCOM TWI peripheral callback function. The FLEXCOM TWI peripheral will call back the client's function with this signature when the FLEXCOM TWI Transfer has completed.
Precondition
FLEXCOMx_TWI_Initialize must have been called for the given FLEXCOM TWI peripheral instance and FLEXCOMx_TWI_CallbackRegister must have been called to set the function to be called. The callback register function should have been called before a I2C transfer has been initiated.
Parameters
Param | Description |
---|---|
context | Allows the caller to provide a context value (usually a pointer to the callers context). |
Returns
None.
Example
void FLEXCOM0_TWI_Callback(uintptr_t context) { if(FLEXCOM0_TWI_ErrorGet() == FLEXCOM_TWI_ERROR_NONE) { //Transfer is completed successfully } else { //Error occurred during transfer. } } // Register Callback function which is defined above FLEXCOM0_TWI_CallbackRegister(FLEXCOM0_TWI_Callback, (uintptr_t)NULL);
Remarks
None