1.12.3.5 CANx_MessageReceive Function
C
The prototype of CANx_MessageReceive() varies based on device family. Refer to the generated header file for the actual prototype to be used.
bool CANx_MessageReceive(uint32_t *id, uint8_t *length, uint8_t *data, uint16_t *timestamp, uint8_t fifoNum, CAN_MSG_RX_ATTRIBUTE *msgAttr) // x - Instance of the CAN peripheral bool CANx_MessageReceive(uint32_t *id, uint8_t *length, uint8_t *data, uint32_t *timestamp, uint8_t fifoNum, CANFD_MSG_RX_ATTRIBUTE *msgAttr) // x - Instance of the CAN peripheral bool CANx_MessageReceive(uint32_t *id, uint8_t *length, uint8_t *data, uint16_t *timestamp, CAN_MAILBOX_RX_ATTRIBUTE mailboxAttr, CAN_MSG_RX_ATTRIBUTE *msgAttr) // x - Instance of the CAN peripheral bool CANx_MessageReceive(uint8_t bufferNumber, CAN_RX_BUFFER *rxBuffer) // x - Instance of the CAN peripheral
Summary
Receives a message from CAN bus.
Description
This routine receives a message from CAN bus.
Precondition
CANx_Initialize must have been called for the associated CAN instance.
Parameters
Param | Description |
---|---|
id | Pointer to 11-bit / 29-bit identifier (ID) to be received. |
length | Pointer to data length in number of bytes to be received. |
data | Pointer to destination data buffer |
timestamp | Pointer to Rx message timestamp, timestamp value is 0 if Timestamp is disabled |
fifoNum | FIFO number |
mailboxAttr | Mailbox type either RX Mailbox or RX Mailbox with overwrite |
msgAttr | Data frame or Remote frame to be received |
bufferNumber | Rx buffer number |
rxBuffer | Pointer to Rx buffer |
Returns
Request status. true - Request was successful.
false - Request has failed.
Example
uint8_t rx_message[8], rx_messageLength; uint32_t rx_messageID; CAN_MSG_RX_ATTRIBUTE msgAttr; CAN1_Initialize(); CAN1_MessageReceive(&rx_messageID, &rx_messageLength, rx_message, 0, 1, &msgAttr);
uint8_t rx_message[8], rx_messageLength; uint32_t rx_messageID; CANFD_MSG_RX_ATTRIBUTE msgAttr; CAN1_Initialize(); CAN1_MessageReceive(&rx_messageID, &rx_messageLength, rx_message, 0, 2, &msgAttr);
uint8_t buf[8], id, length; uint16_t timestamp = 0; CAN_MSG_RX_ATTRIBUTE msgAttr; CAN0_Initialize(); CAN0_MessageReceive(&id, &length, buf, ×tamp, CAN_MAILBOX_DATA_FRAME_RX_OVERWRITE, &msgAttr);
uint8_t rxBuffer[CAN0_RX_BUFFER_SIZE]; memset(rxBuffer, 0x00, CAN0_RX_BUFFER_ELEMENT_SIZE); // Read message from Rx Buffer 0 CAN0_MessageReceive(0, (CAN_RX_BUFFER *)rxBuffer);
Remarks
None.