1.5.24.7 SDADC_ConversionSequenceIsFinished Function
C
bool SDADC_ConversionSequenceIsFinished( void )
Summary
Returns the status of automatic sequence conversion.
Description
This function checks the status of the conversion sequence.
Precondition
SDADC_Initialize() function must have been called first for the associated instance.And conversion must have been started.
Parameters
None.
Returns
true - all the enabled channels in the sequence have finished conversion false - sequence conversion is ongoing
Example
bool seq_status; SDADC_Initialize(); SDADC_ConversionStart(); seq_status = SDADC_ConversionSequenceIsFinished();
Remarks
This function is valid only if auto sequence feature is enabled.