1.5.24.5 SDADC_ConversionResultIsReady Function
C
bool SDADC_ConversionResultIsReady( void )
Summary
Returns the status of the conversion.
Description
This function returns the status of whether conversion is complete.
Precondition
SDADC_Initialize() function must have been called first for the associated instance. Also conversion must have been started.
Parameters
None.
Returns
true - Conversion is not yet finished or not started yet false - Conversion is complete
Example
bool sdadcConversionStatus; SDADC_Initialize(); SDADC_ConversionStart(); sdadcConversionStatus = SDADC_ConversionResultIsReady();
Remarks
This function should be called only after conversion is started.