1.1.10.9 RTOSTimer_FrequencyGet Function

C

uint32_t RTOSTimer_FrequencyGet(void)

Summary

Returns the input frequency of the RTOS timer

Description

Returns the input frequency of the RTOS timer

Precondition

RTOSTimer_Initialize() function must have been called first.

Parameters

None

Returns

Input frequency of the RTOS timer

Example

uint32_t freq = RTOSTimer_FrequencyGet();

Remarks

None