1.22.22.16 RNG_NumGen2Set Function

C

void RNG_NumGen2Set (uint32_t numgen);

Summary

Loads a value into the RNGNUMGEN2 register.

Description

This function can be used to set an initial seed value for the PRNG. When the PRNG operation is finished, RNGNUMGEN2 register contains the MSB 32-bits of the current random number in the PRNG.

Precondition

None.

Parameters

Value to be loaded into RNGNUMGEN2 register.

Returns

None.

Example

RNG_NumGen2Set(0x0d0e0f10);

Remarks

None.