1.22.22.15 RNG_NumGen1Set Function
C
void RNG_NumGen1Set (uint32_t numgen);
Summary
Loads a value into the RNGNUMGEN1 register.
Description
This function can be used to set an initial seed value for the PRNG. When the PRNG operation is finished, RNGNUMGEN1 register contains the LSB 32-bits of the current random number in the PRNG.
Precondition
None.
Parameters
Value to be loaded into RNGNUMGEN1 register.
Returns
None.
Example
RNG_NumGen1Set(0x090a0b0c);
Remarks
None.