1.24.18.16 RNG_NumGen2Set Function
C
void RNG_NumGen2Set (uint32_t numgen);
Summary
Loads a value into the RNGNUMGEN2 register.
Description
This function can be used to set an initial seed value for the PRNG. When the PRNG operation is finished, RNGNUMGEN2 register contains the MSB 32-bits of the current random number in the PRNG.
Precondition
None.
Parameters
Value to be loaded into RNGNUMGEN2 register.
Returns
None.
Example
RNG_NumGen2Set(0x0d0e0f10);
Remarks
None.