1.10.1.18 ADCHS_DMAResultBaseAddrSet Function
C
void ADCHS_DMAResultBaseAddrSet(uint32_t baseAddr)
Summary
Registers the user-defined RAM address at which the DMA engine will start saving the converted data
Description
Registers the user-defined RAM address at which the DMA engine will start saving the converted data
Precondition
ADCHS_Initialize() must have been called first for the associated instance.
Parameters
Param | Description |
---|---|
baseAddr | Physical address of the user-defined RAM address |
Returns
None.
Example
__COHERENT uint16_t adcResultBuffer[4];
ADCHS_DMAResultBaseAddrSet((uint32_t)KVA_TO_PA(adcResultBuffer));
Remarks
None