1.10.1.8 ADCHS_ChannelConversionStart Function

C

void ADCHS_ChannelConversionStart(ADCHS_CHANNEL_NUM channel)

Summary

Starts the ADC conversion of an analog channel

Description

This function starts ADC conversion of an analog channel specified in channel.

Precondition

ADCHS_Initialize() function must have been called first for the associated instance and ADC module corresponding to channel must have been enabled using ADCHS_ModulesEnable() function.

Parameters

Param Description
channel analog channel

Returns

None.

Example

ADCHS_Initialize();
ADCHS_ModulelsEnable(ADCHS_MODULE0_MASK);
ADCHS_ChannelConversionStart(ADCHS_CH0);

Remarks

This function can be called at the start to generate initial trigger. This can also be used to trigger the conversion of an input without changing the trigger source.