1.19.7.6 EVIC_SourceStatusSet Function

C

void EVIC_SourceStatusSet( INT_SOURCE source )

Summary

Sets the status of the interrupt flag for the selected source.

Description

This function sets the status of the interrupt flag for the selected source. This function will not be used during normal operation of the system. It is used to generate test interrupts for debug and testing purposes.

Precondition

EVIC_Initialize() function must have been called first.

Parameters

Param Description
source One of the possible values from INT_SOURCE.

Returns

None.

Example

EVIC_SourceStatusSet(INT_SOURCE_CORE_TIMER);

Remarks

This function implements an operation of the SourceFlag feature. This feature may not be available on all devices. Please refer to the specific device data sheet to determine availability.