1.19.7.3 EVIC_SourceDisable Function
C
void EVIC_SourceDisable( INT_SOURCE source );
Summary
Disables the interrupt source.
Description
This function disables the given interrupt source.
Precondition
EVIC_Initialize() function must have been called first.
Parameters
Param | Description |
---|---|
source | One of the possible values from INT_SOURCE. |
Returns
None.
Example
EVIC_SourceDisable(INT_SOURCE_CORE_TIMER);
Remarks
This function implements an operation of the SourceControl feature. This feature may not be available on all devices. Please refer to the specific device data sheet to determine availability.