1.6.25.40 TCCx_CompareFrequencyGet Function
C
/* x = TCC instance number */
uint32_t TCCx_CompareFrequencyGet( void );
Summary
Provides the given timer's counter-increment frequency.
Description
This function provides the frequency at which the given counter increments. It can be used to convert differences between counter values to real time or real-time intervals to timer period values.
Precondition
TCCx_CompareInitialize() function must have been called first.
Parameters
None.
Returns
Frequency (in Hz) at which the timer's counter increments.
Example
uint32_t frequency = 0;
TCC0_CompareInitialize();
frequency = TCC0_CompareFrequencyGet();
Remarks
None.