1.25.10.21 PIO_PinInterruptDisable Function

C

void PIO_PinInterruptDisable(PIO_PIN pin)

Summary

Disables IO interrupt on selected IO pin.

Description

This function disables IO interrupt on selected IO pin.

Precondition

Corresponding pin must be configured in interrupt mode in MHC Pin Manager. PIO_Initialize() must have been called.

Parameters

Param Description
pin One of the IO pins from the enum PIO_PIN

Returns

None.

Example

PIO_PinInterruptDisable(PIO_PIN_PB3);

Remarks

None.