1.29.23.39 SERCOMx_SPI_Write Function
C
/* x = SERCOM instance number */
/* SPI master mode */
bool SERCOMx_SPI_Write(void* pWrBuffer, size_t txSize)
/* x = SERCOM instance number */
/* SPI slave mode */
size_t SERCOMx_SPI_Write(void* pWrBuffer, size_t txSize )
Summary
Writes data to SERCOM SPI peripheral.
Description
SPI master mode
This function writes "txSize" number of bytes on SERCOM x SPI module. Data pointed by pWrBuffer is transmitted. When interrupt is disabled, this function will be blocking in nature. In this mode, the function will not return until all the requested data is transferred. The function returns true after transferring all the data. This indicates that the operation has been completed. When interrupt is enabled, the function will be non-blocking in nature. The function returns immediately. The data transfer process continues in the peripheral interrupt. The application specified transmit buffer is owned by the library until the data transfer is complete and should not be modified by the application till the transfer is complete. Only one transfer is allowed at any time. The application can use a callback function or a polling function to check for completion of the transfer. If a callback is required, this should be registered prior to calling the SERCOMx_SPI_WriteRead() function. The application can use the SERCOMx_SPI_IsBusy() to poll for completion of transfer.
SPI slave mode
This function writes "txSize" number of bytes on SERCOM x SPI module. Data pointed by pWrBuffer is transmitted. This function returns immediately after copying the data pointed by pWrBuffer into the PLIB's internal buffer. The actual data transfer happens when a SPI transfer is initiated by the SPI master. Upon completion a callback is given to the application.
Precondition
The SERCOMx_SPI_Initialize function must have been called.
SPI master mode
Callback can be registered using SERCOMx_SPI_CallbackRegister API if the PLIB is configured in Interrupt mode and transfer completion status needs to be communicated back to application via callback.
SPI slave mode
Callback must have been registered using SERCOMx_SPI_CallbackRegister API to get notified when the transfer is complete.
Parameters
SPI master mode
Param | Description |
---|---|
pWrBuffer | Pointer to the buffer containing the data which has to betransmitted. For 9 bit mode, data should be right aligned in the 16 bit memory location. In "Interrupt Mode", this buffer should not be modified after calling the function and before the callback function has been called or the SERCOMx_SPI_IsBusy() function returns false. |
txSize | Number of bytes to be transmitted. This value is always the bytecount of the buffer. For 9 bit data length, this should be an even number. |
SPI slave mode
Param | Description |
---|---|
pWrBuffer | Pointer to the buffer where the data must be copied to the PLIB's internal buffer |
txSize | Number of bytes to copy. For 9-bit mode, the txSize must be specified in terms of 16-bit words. |
Returns
SPI master mode
true - If configured for Non-interrupt mode, the function has transmitted the requested number of bytes. If configured for Interrupt mode, the request was accepted successfully and will be processed in the interrupt. false - If pWrBuffer is NULL or txSize is 0. In Interrupt mode, the function will additionally return false if there is an on-going data transfer at the time of calling the function.
SPI slave mode
Returns the number of bytes (or 16-bit words if PLIB is in 9-bit mode) actually copied into the pWrBuffer
Example
SPI master mode
uint8_t txBuffer[4]; size_t txSize = 4; void APP_SPITransferHandler(uintptr_t context) { //Transfer was completed without error, do something else now. } SERCOM0_SPI_Initialize(); SERCOM0_SPI_CallbackRegister(&APP_SPITransferHandler, (uintptr_t)NULL); if(SERCOM0_SPI_Write(&txBuffer, txSize)) { // request got accepted } else { // request didn't get accepted, try again later with correct arguments }
SPI slave mode
uint8_t APP_TxData[4]; uint8_t APP_RxData[10]; size_t txSize = 4; void SPIEventHandler(uintptr_t context ) { if (SERCOM0_SPI_ErrorGet() == SPI_SLAVE_ERROR_NONE) { // Read out the received data. This could be meaningful data if SPI master is // writing to slave or it could be dummy data if SPI master is reading from slave. // However, irrespective of whether slave is expecting meaningful data or dummy // data from master, SPI slave must always read out the data to clear the PLIB's // internal receive buffer. appData.nBytesRead = SERCOM0_SPI_Read(APP_RxData, SERCOM0_SPI_ReadCountGet()); } else { // Handle error } } SERCOM0_SPI_CallbackRegister(SPIEventHandler, (uintptr_t) 0); SERCOM0_SPI_Write(APP_TxData, txSize);
Remarks
SPI slave mode
This function returns immediately. Application must register a callback to get notified, when the data transfer is complete. A data transfer is considered as complete, when the Chip Select line is driven to inactive state by the SPI master.